|
Markers |
|
Choices: Start | Pulse per second | Pulse per millisecond
Default: Marker 1—Start, Marker 3—Pulse per second, Marker 4—Pulse per millisecond
Select the signal pattern for the marker output. The marker output signal is mapped to a rear panel connector on the signal generator.
On an ESG:
Marker 1 correlates to the EVENT1 output connector and the AUX IO connector
Marker 3 and Marker 4 correlate to only the AUX IO connector
On an EXG/MXG, all three marker signals are available at the rear panel AUX IO connector, or use the front panel to route two of the marker signals to the following rear panel connectors (one signal per connector):
EVENT 1 (marker 1 is the default setting for this connector)
TRIG OUT
For more information on the signal generator rear-panel connectors and marker output signals, see the signal generator's User Guide.
Range: –1 ms to 1 ms (resolution of 15 ns)
Default: 0 ns
Enter a value to offset the timing of the markers that use either the or choices. A positive value delays the timing of the marker signal and a negative value advances the timing.