Use the Marker Source Selection drop-down menu for the or cells to set active marker points within the waveform. The cells are located in the parameter configuration table.
| Frame Start |
Sets the first five marker bits of the waveform to 1 to indicate the beginning of the waveform. (Sets an active marker for the first five waveform samples.)
Sets the first five marker bits of the frame to 1 to indicate the beginning of each frame in the waveform. (Sets an active marker for the first five frame samples.)
Activates the automatic leveling control (ALC) function. When enabled, the ALC monitors and controls the RF output power of the signal generator. Use the following links to access more details:
The marker bits are set to 1 within ALC Control part in the waveform.
Assigns a specific marker to activate RF blanking. ALC hold is automatically enabled during output blanking.
The marker bits are set to 1 for all non-zero sample points to indicate the burst part in the waveform.
When using this selection with an 802.15.4 O-QPSK BPSK signal, the following conditions must be true for RF blanking to occur:
Number of Frames is greater than one
Idle Interval is greater than zero
For more on how RF Blanking Control is used with an 802.15.4 O-QPSK BPSK signal, see the concept topic.