To generate signals using the N7610B Signal Studio for Short Range Communications software, you must have a properly configured PC and a properly configured instrument, as described in the following tables.
|
Instruments |
Requirements |
|---|---|
|
N5172B EXG X-Series RF vector signal generator |
Firmware revision B.01.10 or later (how to upgrade) Required options: N5172B-503 (9 kHz to 3 GHz frequency range) N5172B-653 (Internal baseband generator, 32 MSa/sec, up to 60 MHz RF bandwidth) Recommended options: N5172B-009 (internal Flash drive) |
|
N5182B MXG X-Series RF vector signal generator |
Firmware revision B.01.10 or later (how to upgrade) Required options: N5182B-503 (9 kHz to 3 GHz frequency range) N5182B-656 (Internal baseband generator, 32 MSa/sec, up to 80 MHz RF bandwidth) Recommended options: N5182B-009 (internal Flash drive) |
|
N5182A MXG RF vector signal generator |
Firmware revision A.01.20 or later (how to upgrade) Required options: N5182A-503 (9 kHz to 3 GHz frequency range) N5182A-651 (Internal baseband generator, 30 MSa/sec, up to 24 MHz RF bandwidth ) Recommended options: N5182A-019 (Increase Baseband Generator Memory to 64MSa) |
|
E4438C ESG vector signal generator |
Firmware revision C.04.95 or later (how to upgrade) Required options: E4438C-503 (250 kHz to 3 GHz frequency range) E4438C-601 (internal baseband generator with 8 Msample memory and digital bus capability) Recommended options: E4438C-602 (internal baseband generator with 64 Msample memory and digital bus capability) |
|
E8267D PSG vector signal generator |
Firmware revision C.04.92 or later (how to upgrade) Required options: E8267D-520 (250 kHz to 20 GHz frequency range) E8267D-602 (internal baseband generator with 64 Msample memory and digital bus capability) Recommended options: E8267D-005 (6 GB internal hard drive) |
|
M9381A PXIe vector signal generator |
Driver version: 1.4.400.0 or later
Required options: M9381A-F03 (1 MHz to 3 GHz frequency range) M9381A-B04 (40 MHz modulation bandwidth) M9381A-M01 (32 MSa memory) M9381A-300 (add M9300A PXIe frequency reference) Limitations: The M9381A VSG has a limitation related to the Power Search and DC Cal functions, creating a time-synchronization loss. That is, the signal timing changes after a Power Search or DC Cal. When ALC is set to Off, Signal Studio automatically runs Power Search, which affects the user's trigger signal for starting waveform playback. Even though the timing alignment of the trigger signal and waveform are properly set, the Power Search function disrupts this synchronization. In these cases, use the following workarounds:
For DC Cal, run it before you download and play the waveform. Do not run DC Cal while the signal is playing, which disrupts the synchronization. |
200 GB HDD with 2 GB free disk space at runtime (5 GB or higher recommended)
1024 x 768 screen resolution (1280 x 1024 recommended)
Windows 7 (Professional/Ultimate/Enterprise)1,2:
1 GHz or faster 32-bit or 64-bit processor
1 GB of memory minimum for the 32-bit version
2 GB of memory minimum for a 64-bit version
1.5 GB hard disk space (includes 1 GB for Microsoft .NET Framework and 65 MB for the Keysight IO Libraries)
Microsoft Internet Explorer (8.0 or later)
Microsoft .NET Framework 3.5 or .NET Framework 3.5 Service Pack 1 (included with Windows 7) (2. Downloading and Installing the .NET Framework)
Keysight IO Libraries, version 15.5 or later (3. Downloading and Installing the Keysight IO Libraries Suite)
Keysight License Manager (4. Downloading and Installing the Keysight License Manager )
128 MB graphics memory with DirectX 9 graphics support (recommended)
Windows XP Service Pack 3 or later (Professional)
2 GHz Pentium 4 or higher (recommended)
512 MB of memory minimum (1.0 GB or higher recommended)
1.5 GB hard disk space (includes 1 GB for Microsoft .NET Framework and 65 MB for the Keysight IO Libraries)
Microsoft Internet Explorer (6.0 or later)
Microsoft .NET Framework 3.5 or .NET Framework 3.5 Service Pack 1 (2. Downloading and Installing the .NET Framework)
Keysight IO Libraries, version 15.5 or later (3. Downloading and Installing the Keysight IO Libraries Suite)
Keysight License Manager (4. Downloading and Installing the Keysight License Manager )
Installed GPIB IO interface card, LAN interface card, or USB/GPIB interface connector
Keysight VISA
Microsoft Windows Installer version 2.0 or later
1 No support for Itanium64.
2 Signal Studio is compatible with the 64-bit operating system, but performs at the 32-bit speed.