Real Time

Waveform Graph

Click Waveform Setup in the Closedtree view. The graph view is located at the bottom of the Waveform Setup and Carrier nodes. For multiple antenna configurations, a tab for each antenna port is displayed above the graph view. Click the tab of the antenna port for which you want to view a waveform graph. Click the Waveform tab to display the waveform graph.

Click Generate or Download from the main tool bar to generate an I/Q waveform and plot four different waveform graphs (Power, I+Q, I/Q, and Spectrum) of the current waveform configuration. Changes to the waveform configuration do not appear on the graph until you generate the waveform. The status bar at the bottom of the screen shows waveform generation progress.

The Power plot is shown in the Figure.

Figure. Power plot

Click the down arrow to open a Closeddrop-down menu from which you can select different waveform plots. Selections include Power (shown above), I+Q, I|Q, and Spectrum. Click the button to the left of the arrow to select the next plot type in the list without displaying the menu.

CCDF Graph