|
1. Basic |
2. Markers |
|---|---|
| Number of Frames | |
| Oversampling Ratio | |
| Waveform Length | |
| PHY Specification |
Enter an alpha-numeric waveform file name. The maximum name length is 23 characters (such as E4438C, N5182A and etc.).
If you enter a name with more than 23 characters, the software truncates the name to 23 characters when you click outside of the cell. The name can include spaces and the following special characters: _ $ & # + - [ ].
Enter an alpha-numeric comment of up to 32 characters. The comment resides in the file header and can include spaces and special characters.
Range: 1–2000
Default: 1
Enter the number of frames for use in the waveform.
Range: 2–64
Default: 16
Enter the oversampling ratio of the waveform. The Waveform Length and Total Sample Points are automatically determined based on the oversampling ration.
Displays the number of sample points in the waveform. You cannot edit this cell. The parameter is directly related to the oversampling ratio value selected. (Increasing the oversampling ratio increases the total sample points.)
Displays the waveform length that are included in the waveform. You cannot edit this cell. The parameter is related to the number of frames. (Increasing the number of frames increases the waveform length.)
Choices: 802.15.4g MR-FSK | 802.15.4g MR-OFDM | 802.15.4 | ITU-T G.9959
Default: 802.15.4g MR-FSK
Select the format of PHY Specification of the waveform. For more information, use the following links:
Default: Waveform Start
Configure the marker points for Marker 1 using the Marker Source Selection drop-down menu.
The signal generator outputs the Marker 1 signal from the rear-panel EVENT 1 output. For more information, see the signal generator's User Guide.
Default: Frame Start
Configure the marker points for Marker 2 using the Marker Source Selection drop-down menu.
The signal generator outputs the Marker 2 signal from the rear-panel EVENT 2 output. For more information, see the signal generator's User Guide.
Displays the source for Marker 3.
Display the source for Marker 4.
The graph view displays several different representations of the generated waveform. For more information, see Graph View.