Carrier Setup

1. Basic

2. FM

3. Audio

4. RDS

State

Frequency Offset

Initial Phase

Power

FM Deviation

FM Deviation Unit

Normalized

Pilot

Pilot Deviation

Pilot Frequency

Pilot Initial Phase

Stereo Frequency

Stereo Initial Phase

Audio Deviation

Audio Source Pattern

Audio Source

Left Tone(s)

Right Tone(s)

Pre-emphasis

Normalized Audio Frequency

RDS

RDS Deviation

RDS Frequency

RDS Initial Phase

RDS Filter Type

Alpha

RDS Payload

1.Basic

State

Choice: On | Off

Default: On

Double-click or use the drop-down menu to set the state of the carrier ON or OFF.

Frequency Offset

Range: -12.5 to 12.5 MHz

Default: 0.000000 Hz

Set the frequency offset for the carrier relative to the signal generator’s frequency setting.

Initial Phase

Range: 0.00 to 359.00 deg

Default: 0.00 deg

Set the initial phase of the carrier.

Power

Range: -50.00 to 0.00 dB

Default: 0.00 dB

Set the carrier’s power relative to the signal generator’s amplitude setting.

2.FM

FM Deviation

Range: 1Hz to 300 kHz

Default: 75.000 kHz

Frequency deviation is used in FM radio to describe the maximum instantaneous difference between an FM modulated carrier frequency, and the nominal carrier frequency.

FM Deviation Unit

Choice: Percentage | Frequency

Default: Percentage

Double-click or use the drop-down menu to set the FM Deviation Unit to percentage or frequency. Pilot Deviation and RDS Deviation will be set in the selected FM Deviation Unit accordingly.

Normalized

Choice: True | False

Default: True

Double-click or use the drop-down menu to select whether the FM deviation is normalized. This key is only visible when FM Deviation Unit is set to percentage.

Pilot

Choice: On | Off

Default: On

Set pilot status.

When transmitted in stereo, it's preferable to synchronize the RDS subcarrier with the 19 kHz pilot signal, rather than leave these two signals in complete independence. In fact substantial inter-modulation may be produced between the 3rd harmonic of the pilot signal and the RDS signal, generating an unwanted beat which may be audible.

The following picture shows the baseband layout of FM broadcasting:

Pilot Deviation

Range: 0.1% to 20%

Default: 10.0 %

The percentage of frequency deviation, since the tolerance on the frequency of the 19 kHz pilot-tone is from -2 Hz to 2 Hz.

Pilot Frequency

Range: 14.000 kHz to 24.000 kHz

Default: 19.000 kHz

In FM stereo broadcasting, a pilot tone of 19 kHz indicates that there is stereophonic information at 38 kHz (19×2, the second harmonic of the pilot). The receiver doubles the frequency of the pilot tone and uses it as a phase reference to demodulate the stereo information.

Pilot Initial Phase

Range: 0.00 deg to 359.00 deg

Default: 0.00 deg

Set the initial phase of the pilot signal.

Stereo Frequency

Range: 34.000 kHz to 42.000 kHz

Default: 38.000 kHz

Set the stereo frequency.

Stereo Initial Phase

Range: 0.00 deg to 359.00 deg

Default: 0.00 deg

Set the initial phase of the stereo signal.

3.Audio

Audio Deviation

Range: 1% to 100%

Default: 100 %

Set the percentage of audio deviation.

Audio Source Pattern

Choice: L Only | R Only | L = R | L = -R | L ≠ R

Default: L = R

Select the type of audio source.

Audio Source

Choice: Tones | Wav File

Default: Tones

Set the format of audio source, which could be Tones or Wav File. Notice that Pre-emphasis is effective only when audio source is multi-tone.

Wav File can only be enabled when Normalized is True.

Left Tone (s)

Set the tone (s) of the left channel in the following procedures.

Click on the cell of Left Tone (s) , and a will appear on the right end of the cell. Click on the button, and a dialog for multi-tone configuration will pop up. 

Add a tone

Click on button, a new tone with default frequency and amplitude will be generated.

Remove a tone

Click on button, an existing tone will be eliminated. Notice that the items on top will be removed first.

Add multitone

Click on button, a list of tones with configured frequencies and amplitudes will be displayed. You can specify the Start frequency, Step, End frequency and Amplitude through the Closeddialog on the right side, here Step has been set to 4kHz as an example.

Right Tone (s)

Set the tone(s) of the right channel. For more information about the procedures, please refer to the Left Tone (s) setup.

Pre-emphasis

Choice: Off | 50 us | 75 us

Default: Off

In FM transceiver, pre-emphasis and de-emphasis is always adopted to solve the low SNR problem of high frequency band. Pre-emphasis refers to raising high frequency components of the input signal at the transmitter side.

However, the maximum frequency deviation after FM may increase since the high frequency components has been lifted, and it might exceed the spectrum width allowed by the original channel. That’s why the signal ought to be attenuated after pre-emphasis, before modulation, in order to keep the frequency deviation constant.

When Pre-emphasis is turned on and Normalized is true, the audio signal will pass a filter shown in Figure 1. When Normalized is false and Normalized Audio Frequency cell is set to a value (for example, 15 kHz), the pre-emphasis gain is 0dB at 15 kHz. That means the values of y-Axis in the Figure 1 will be normalized by 13.66dB. This case is commonly used because the input range of VCO is limited.

Figure 1 The relationship curve between Frequency and Gain (50us)

Normalized Audio Frequency

Default: 15.000 kHz

Sets the normalized audio frequency. This value will affect the pre-emphasis filter used. For more details, refer to Pre-emphasis.

This cell is only visible when Normalized is set to false and Pre-emphasis is turned on.

4.RDS

RDS

Choice: On |Off

Default: On

Radio Data System, or RDS, is a standard from the European Broadcasting Union for sending small amounts of digital information.

RDS Deviation

Range: 0.1% to 20%

Default: 6.0%

RDS Frequency

Range: 53 to 61 kHz

Default: 57 kHz

RDS Initial Phase

Range: 0.00 deg to 359 deg

Default: 0.00 deg

RDS Filter Type

Choice: Nyquist | Root Nyquist

Default: Root Nyquist

Set the filter type of RDS.

Alpha

Range: 0.05 to 1

Default: 1

Set the roll-off factor of a root raised cosine filter or a raised cosine filter.

RDS Payload

Choice: Messages | Pattern Bits

Default: Messages

Set the RDS payload type.

RDS Pattern Bits

Choice: All 1s| All 0s| User defined

Default: All 1s

Set the RDS pattern bits.

RDS Insert CRC

Double-click or use the drop-down menu to set whether the CRC (Cyclic redundancy check) is inserted into the RDS pattern bits.