Double-click or use the drop-down menu to control the operating state of the carrier.
Range: -10 MHz to 10 MHz
Set the frequency offset of this carrier. Frequency offset is the difference between this carrier and the frequency of signal generator in the instrument node.
Shows the frequency of this carrier. This is read only and calculated by instrument frequency and frequency offset.
Range: -50.00 to 0.00 dB
Default: 0.00 dB
Set the carrier’s relative power. This is relative power among carriers, which means a carrier with relative power=-10dB is -10dB lower than the carrier with relative power=0dB.
Range: 0 ms to waveform length
Set the relative delay of this carrier.
Shows the the number of frames generated in this wavefrom. This is read only and calculated based on baseband file used.