Status Bar

The status bar updates in real-time to let you know the status of running operations, such as waveform generation. It also displays hardware connectivity information, the total sample points of the waveform and the progress of waveform generation. No hardware connected is displayed until the hardware is connected.  

If "Connecting Hardware..." continues to be displayed and does not change to "Ready" within a few minutes, verify that the   IO Libraries are properly configured for the connected instruments.

Run Status

This area shows the status of the software's setup.

The following are some of the possible run status messages:

Generating

Generating the waveform points according to the waveform setup of this project.

Generated

The required waveform has already been generated.

Downloading

Downloading the waveform to instrument as configured in Hardware.

Download

The required waveform has already been Downloaded.

Connection Status

This area shows the connection status of the software to the signal generator.

The following are some of the possible connection status messages:

Blank (no text)

Simulated hardware mode.

Connected

The instrument connection is checked and verified.

Not Connected

The software is not connected to the signal generator at this moment.