View popup View Popup View Popup View Popup View Popup View Popup Go to description Go to description Go to description Go to description Go to description

XM Satellite Radio

1. Baseband File

Baseband File Type

Choices: Demo File | Keysight Baseband File

Select Demo File or Keysight Baseband File to use the input of physical layer.

[:SOURce]:RADio:XM[:BBG]:BFILe:TYPe Demo File | Keysight Baseband File

[:SOURce]:RADio:XM[:BBG]:BFILe:TYPe ?

File Location

Choice: Local | Instrument

Default: Local

Double-click or use the drop-down menu to select where the payload is. The Local is recommended.

File Name

The name of the baseband file. Click the right button to select and open a tdm_k or tdmh_k file.

tdm_k file is for non-overlay setting and tdmh_k file can work for both overlay and non-overlay case. Contact Keysight or SiriusXM for more information.

[:SOURce]:RADio:XM[:BBG]:BFILe:FILe <File Location>

[:SOURce]:RADio:XM[:BBG]:BFILe:FILe ?

Number of Master Frames

Number of frames calculated from the file.

[:SOURce]:RADio:XM[:BBG]:BFILe:FRAMe <val>

[:SOURce]:RADio:XM[:BBG]:BFILe:FRAMe ?