Installation Steps: 1 2 3 4 5 6 7
Turn on the instrument and the computer.
Start the Signal Studio software.
Establish communications between the software and the
instrument by first selecting in the
Welcome
to Keysight Signal Studio... dialog box
(System Configuration Wizard) that appears.
Click and follow the remaining prompts. (Be prepared to enter the instrument's IP/GPIB address.)
If you are running Signal Studio on the PXB, use ”localhost” in the Hostname/IP Address field in Step 4 of the System Configuration Wizard.
If you are running Signal Studio on a PC connected to the PXB, use the PXB's address (LAN/GPIB) or hostname (LAN only)
hostname: click > and view the Machine Name row
IP address: click > and view the IP Address row
GPIB address: click >
If you are running Signal Studio on a PC connected to an EXT, use the EXT's address (LAN/GPIB) or hostname (LAN only) [Some Signal Studio products do not support live connectivity to the EXT]:
hostname: press > > and view the Computer Name row
IP address: press > > and view the IP Address row
GPIB address: press > >
If you are running Signal Studio on a PC connected to a signal generator, refer to the following table to locate the instrument's address (LAN/GPIB) or hostname (LAN only):
|
Connection |
Signal Generator |
Key Path |
|---|---|---|
|
LAN |
EXG and MXG1 |
> > > |
|
ESG PSG |
> > |
|
|
GPIB |
EXG and MXG |
> > . |
|
ESG PSG |
> > |
1 Signal Studio accepts either the LAN address or hostname. So if you want to use the hostname, just enter the hostname into the software's Hostname/IP Address field.
If the connection fails or for help with error messages, refer to Troubleshooting.
After making the connection, you can view the instrument's information by selecting in the tree view.
Install the software license.
To learn about the different licenses, see Licensing.
To install the license, see Installing the License.