Real Time

Waveform Graph

Click Generate or Download from the main tool bar to generate an I/Q waveform and plot four different waveform graphs (Power, I+Q, I/Q, and Spectrum) in accordance with the current channel configuration. Any changes to the channel configuration do not appear on the graph until you generate the waveform. The status bar at the bottom of the screen shows waveform generation progress.

Power plot shows the cumulative power of the carrier configuration.

The Waveform and CCDF graphs are minimized in the Carrier node' s initial view. To view the graphs, click and drag the border above the CCDF and Waveform graphs.

CCDF Graph

Waveform Setup