The N7612C Signal Studio for TD-SCDMA/HSPA 2018 software can be installed on a PC for use with the N5172B EXG or N5182B MXG X-series signal generators. The PC software allows the user to configure settings, generates scenario data, and provides a user interface for real-time control of the signals being produced by the signal generators.
|
Instruments |
Requirements |
|---|---|
|
N5172B EXG X-Series RF vector signal generator |
Firmware:
Required options:
Recommended options:
N5172B-660 is not required for the N7609B software's basic option. |
|
N5182B MXG X-Series RF vector signal generator |
Firmware:
Required options:
Recommended options:
N5182B-660 is not required for the N7609B software's basic option. |
|
E8267D PSG vector signal generator |
Firmware:
Required options:
Recommended options:
|
|
M9381A PXIe vector signal generator |
Driver:
Recommended options:
Limitations: The M9381A VSG has a limitation related to the Power Search and DC Cal functions, creating a time-synchronization loss. That is, the signal timing changes after a Power Search or DC Cal. When ALC is set to Off, Signal Studio automatically runs Power Search, which affects the user's trigger signal for starting waveform playback. Even though the timing alignment of the trigger signal and waveform are properly set, the Power Search function disrupts this synchronization. In these cases, use the following workarounds:
For DC Cal, run it before you download and play the waveform. Do not run DC Cal while the signal is playing, which disrupts the synchronization. |
|
E6640A EXM wireless test set |
Software:
Recommended options:
|
200 GB HDD with 2 GB free disk space at runtime (5 GB or higher recommended)
1024 x 768 screen resolution (1280 x 1024 recommended)
If you use a high-resolution display, the GUI's font size may appear too small to read. To resolve this, lower your PC's display resolution, but make sure the display scaling remains set at 100 percent, otherwise portions of the GUI will become truncated and hidden from view.
Windows 10 (64 bit):
1 GHz or faster
2 GB of memory minimum
1.5 GB hard disk space (includes 1 GB for Microsoft .NET Framework and 65 MB for the Keysight IO Libraries)
Microsoft Internet Explorer 11.0 or later
128 MB graphics memory with DirectX 9 graphics support (recommended)
Windows 7 (64 bit):
1 GHz or faster
2 GB of memory minimum
1.5 GB hard disk space (includes 1 GB for Microsoft .NET Framework and 65 MB for the Keysight IO Libraries)
Microsoft Internet Explorer 11.0 or later
128 MB graphics memory with DirectX 9 graphics support (recommended)
Microsoft .NET Framework 4.5.2 or later
Keysight IO Libraries, version 18.0 or later
Keysight License Manager 5 (4. Downloading and Installing Keysight License Manager 5)
Keysight License Service (included with installer)
Keysight Host Processor Platform (included with installer)
Installed GPIB IO interface card, LAN interface card, or USB/GPIB interface connector
Keysight VISA
Microsoft Windows Installer version 2.0 or later
In order for the N7612C Signal Studio for TD-SCDMA/HSPA 2018 software to generate signals, you must have a properly configured PC and properly configured signal generation hardware, all of which meet the system requirements.
|
Instruments |
Requirements |
|---|---|
|
N5172B EXG X-Series RF vector signal generator |
Firmware:
Required options:
Recommended options:
|
|
N5182B MXG X-Series RF vector signal generator |
Firmware:
Required options:
Recommended options:
|
|
N5182A MXG vector signal generator |
Firmware:
One of the following baseband generator options:
One of the following frequency options:
Recommended options:
|
|
E4438C ESG vector signal generator |
Firmware:
One of the following baseband generator options:
One of the following frequency options:
Recommended options:
|
|
M9381A PXIe vector signal generator |
Driver:
Recommended options:
Additional options to consider:
Limitations: The M9381A VSG has a limitation related to the Power Search and DC Cal functions, creating a time-synchronization loss. That is, the signal timing changes after a Power Search or DC Cal. When ALC is set to Off, Signal Studio automatically runs Power Search, which affects the user's trigger signal for starting waveform playback. Even though the timing alignment of the trigger signal and waveform are properly set, the Power Search function disrupts this synchronization. In these cases, use the following workarounds:
For DC Cal, run it before you download and play the waveform. Do not run DC Cal while the signal is playing, which disrupts the synchronization. |
|
E6640A EXM wireless test set |
Software:
Recommended options:
Additional options to consider:
|
|
M9420A VXT PXIe vector transceiver |
Software:
Recommended options:
Additional options to consider:
|
|
M9421A VXT PXIe vector transceiver |
Software:
Recommended options:
Additional options to consider:
|
200 GB HDD with 2 GB free disk space at runtime (5 GB or higher recommended)
1024 x 768 screen resolution (1280 x 1024 recommended)
If you use a high-resolution display, the GUI's font size may appear too small to read. To resolve this, lower your PC's display resolution, but make sure the display scaling remains set at 100 percent, otherwise portions of the GUI will become truncated and hidden from view.
Windows 10 (64 bit):
1 GHz or faster
2 GB of memory minimum
1.5 GB hard disk space (includes 1 GB for Microsoft .NET Framework and 65 MB for the Keysight IO Libraries)
Microsoft Internet Explorer 11.0 or later
128 MB graphics memory with DirectX 9 graphics support (recommended)
Windows 7 (64 bit):
1 GHz or faster
2 GB of memory minimum
1.5 GB hard disk space (includes 1 GB for Microsoft .NET Framework and 65 MB for the Keysight IO Libraries)
Microsoft Internet Explorer 11.0 or later
128 MB graphics memory with DirectX 9 graphics support (recommended)
Microsoft .NET Framework 4.5.2 or later
Keysight IO Libraries, version 18.0 or later
Keysight License Manager 5 (4. Downloading and Installing Keysight License Manager 5)
Keysight License Service (included with installer)
Keysight Host Processor Platform (included with installer)
Installed GPIB IO interface card, LAN interface card, or USB/GPIB interface connector
Keysight VISA
Microsoft Windows Installer version 2.0 or later