Ensure that the cable and all connectors are undamaged.
Ensure that the GPIB cable is securely connected to the PC and the signal generator.
Verify that the GPIB address entered in the software matches that of the signal generator. In the software, click to view the GPIB settings.
Validate the connection. Select an signal generator connection and click . Observe the resultant messages in the and cells to verify that the software is connecting to the signal generator.
Review the GPIB setup section, and the information about installing Keysight I/O libraries.
If you are using a National Instruments (NI) GPIB card and errors occur when you download a waveform, follow steps 1-3 below. If you have both an Keysight and a National Instruments card installed, and you want to use the Keysight card, you will also need to perform steps 4-5.
If using a National Instruments GPIB interface card:
Uninstall any Keysight IO Libraries that you have previously installed.
Ensure that you have both the National Instruments PCI card drivers and VISA drivers installed, and verify that the card is working.
Reinstall Keysight IO Libraries version 14.2. Make sure that Keysight VISA is selected as the secondary VISA (default).
To use an Keysight GPIB interface card if both cards are installed:
Open National's Measurement and Automation Explorer (MAX).
Select Tools > NI-Visa > Visa Options > Passports. Ensure the NiVisaTulip.dll box is checked.
If the signal generator is connected directly to a computer, use a crossover LAN cable; if the signal generator is connected to a network/hub/router, do not use a cross-over LAN cable.
Ensure that the cable and all connectors are undamaged.
Ensure that the LAN cable is securely connected to the PC and the signal generator.
Ensure that the instrument LAN connectors are active: flashing green or yellow lights indicate LAN activity.
Verify that the Hostname or IP address entered in the software matches that of the signal generator. In the software, click to view the LAN settings.
Validate the connection. Select an signal generator connection and click . Observe the resultant messages in the and cells to verify that the software is connecting to the signal generator.
Run the 'ping' program:
On the computer go to > > (or DOS).
At the C:\> prompt, enter ping <IP address>,
where <IP address> is the signal generator's IP address.
If the signal generator does not respond, contact your IT department for help.
If the 'ping' program works correctly, but there is still a connection problem, and the PC is connected directly to the signal generator (using a cross-over cable), add the signal generator's IP address and hostname to the Hosts file, which resides at: C:\Winnt\system32\drivers\etc\Hosts.
In a text editor such as Notepad, open the Hosts file.
Write the IP address for the signal generator and spectrum analyzer at the bottom of the file.
(Refer to the example of a hosts file below.)
Save the file and close the text editor.
Do not use "Save As" when saving the Hosts file; this file does not have a file extension.
# Copyright (c) 1993-1999 Microsoft Corp.
#
# This is a sample HOSTS file used by Microsoft TCP/IP for Windows.
#
# This file contains the mappings of IP addresses to host names. Each
# entry should be kept on an individual line. The IP address should
# be placed in the first column followed by the corresponding host name.
# The IP address and the host name should be separated by at least one
# space.
#
# Additionally, comments (such as these) may be inserted on individual
# lines or following the machine name denoted by a '#' symbol.
#
# For example:
#
# 102.54.94.97 rhino.acme.com # source server
# 38.25.63.10 x.acme.com # x client host
<xxx.xxx.xxx.xxx> localhost
<xxx.xxx.xxx.xxx> <signal generator hostname>
<xxx.xxx.xxx.xxx> <spectrum analyzer hostname>