HSDPA Key Features

In HSDPA mode, key techniques include the use of higher order modulation (16QAM), AMC (Adaptive Modulation and Coding), (Hybrid Automatic Repeat reQuest (H-ARQ), and fast cell search.

Adaptive Modulation and Coding

AMC changes the modulation and coding format in accordance with variations in the channel conditions, subject to system restrictions. The channel conditions can be estimated based on feedback from the receiver. Key advantages of AMC are:

H-ARQ

Using H-ARQ, link layer acknowledgements are used for retransmission decisions instead of explicit measurements as in AMC. The software supports both Chase combining, and incremental redundancy H-ARQ retransmission schemes.