For HSDPA mode, the switching point in the Waveform Setup must be set at 1.
opens a window that allows you to select HS-DSCH RMC QPSK or HS-DSCH RMC 16QAM reference measurement channel as defined in TS 25.222. When selected, the precoded parameters for the channel are automatically set in the HS-DSCH window. Refer to RMC Configuration for details.
This table displays the HSDPA channel and its attributes as currently set. Double-clicking a channel row activates the setup tables for that channel.
Range: 1 to 15
Enter a value to select the
UE category.
All other parameters are automatically set depending on the selected category.
Range: 12, 16 depending on UE category
Displays the maximum number of codes per timeslot as specified by the UE category selection.
Range: Fixed at 5
Displays the maximum number of codes per TTI of HS-DSCH as specified by the UE category selection.
Range: 7008, 10204, 14043 depending on UE category
Displays the maximum number of bits per TTI as specified by the UE category selection.
Range: depends on UE category.
Displays the total soft channel bits as specified by the UE category selection.
Choice: On or Off
Displays whether the UE category supports SF = 1.