This table displays the HSUPA channel and its attributes as currently set. Double-clicking a channel row activates the setup tables for that channel.
Choices: FRC1 | FRC2 | FRC3
Displays the E-DCH fixed reference channel.
Range: 1 to 6
Displays the UE category of the HSUPA channel.
Displays the number of codes per timeslot used by E-PUCH.
Range: Fixed at 5
Displays the maximum number of timeslots per TTI used by HSUPA.
Displays the number of transport channel bits that can be received within an E-DCH TTI.
Choice: True or False
Displays whether the UE category supports SF = 1.
Range: 1 to 5
Displays the number of E-UCCH.