Power Calculation | Channel Power Assignment | RU and Timeslot Power Assignment
The channel power on each timeslot is the same.
When multiple RUs are assigned for each channel, the power ratio of each RU on the multicode configuration is related to the SF of each RU. For example, two RUs (referred to here as RU1 and RU2) are assigned to a channel. Each RU has its own SF. For this configuration, the following is true:
RU1 power : RU2 power = SF of RU2 : SF of RU1
The summed power balance between midambles and the data parts should be the same in each timeslot. If the same midamble is assigned to multiple RUs, the total midamble power is set to 1/n to maintain the power balance within each of the data parts.
The system assigns channel power based on 0 dB in the UI.
Actual power level is set in dBm on the signal generator. The maximum power which is set in the UI is mapped to the signal generator power level with the ALC ON.
For multiple channels that are in the same timeslot and/or have AWGN power applied, the power is additive. The total power value of a timeslot may be exceeded at 0 dB.
For example: If 2 channels, 0 dB channel and 0 dB channel, are combined in the same timeslot, the final power becomes 3 dB. If 3 dB is the maximum power of the power configuration, this 3 dB will be mapped to a signal generator power level. To avoid an over range error, each assigned channel power needs to be recalculated relatively, from 3 dB and the signal generator power level.
The following figure illustrates the power mapping from the UI power setting to the signal generator power output level.
In the basic carrier setup, you can set the RU power relative to the value of the other RUs. Timeslot power is equal to the sum of all the RU powers and can be adjusted relative to the other timeslots as needed.
For example: