3. Executing the Measurement and Viewing Results

This section introduce how to execute the envelope tracking test and how to view the measurement results. Follow the procedure below to execute the measurement and view the measurement results.

Initial Run

Timing Alignment

Executing the Measurement

Viewing the Measurement Results

Initial Run

  1. Once the measurement begins, the detailed information will be displayed in the Log view at the bottom of the window as shown below.

The default Delay setting in Envelope Tracking block may not be the optimal value for the current instruments/DUT connections. So the PA output performance (AM-AM, ACP) may be poor. Further timing alignment between the RF Signal Generator and the Envelope Signal Generator is required.

Timing Alignment

Timing alignment is to synchronize the input signal of the PA (the output of the RF Signal Generator) with the input voltage of the PA (the output of the Envelope Signal Generator) in time domain. There are two methods:

Once sample rate related setting changed, or M8190 was reset manually, the relative timing between envelope signal and RF signal signal will become unknown and unstable, “run” action and “align” action must be repeat again.

If the related settings (e.g. sample rate, IQ delay, trigger delay in Generator instruments, etc.) are changed and applied, it is recommended to do the timing alignment again.

Executing the Measurement

Viewing the Measurement Results

In the measurement view, there are four result windows: AM-AM, AM-PM, ACP, and EVM vs. Power. EVM vs. Power results are displayed only when Power Sweeping (in PA block) is set to On.

For ET test, ACP results are viewed. To view more detailed information, double-click on the ACP window to enlarge it as shown in the figure below.

Figure 1. ACP Results

You can make your own measurements, such as power-added efficiency (PAE) test, based on the PA output signal using the Signal Studio for Power Amplifier Test software, Keysight VSA software or applications on the Signal Analyzer. For information on how to make PAE measurements, see Example PAE Measurements.