Example ET + DPD Measurement

ET is usually used together with DPD to improve the PA performance and efficiency. In this example, ET + DPD measurement is performed. The whole measurement process includes the following three parts.

  1. Setting up the measurement system

  2. Configuring parameters in N7614C Signal Studio for Power Amplifier Test 2022 software

  3. Executing the measurement and viewing the measurement results