Installation Steps: 1 2 3 4 5 6
A Microsoft .NET Framework version may come pre-installed with your Windows operating system. If the pre-installed .NET Framework version is not the same version as stated in the text below, you must install the required version. Different versions of .NET Framework can simultaneously reside on the Windows operating system.
Ensure that you have Microsoft .NET Framework 4.0 or later installed on the Windows operating system (PC or Windows-based instrument) that is to receive the Signal Studio software download. If you know it is already installed, proceed to Installation Step 3.
Before installing .NET Framework 4.0, you can verify whether it is already installed in your PC by doing the following:
Go to > > > .
Look for Microsoft .NET Framework 4.0 or Microsoft .NET Framework 4.0 Client Profile in the list of programs.
If you do not see it listed, you must download it from Microsoft.
If you do not have the .NET Framework 4.0 installed, do the following:
Search the site for .NET Framework 4.0.
Download and install the software.
If you get a security exception message when you try to open the software, consult your system administrator to resolve the problem.