To get the AM-AM, two signals are used. One is the reference signal, which is the PA input signal. The other is the PA output signal, for which the IQ waveform data is captured using the Signal Analyzer.
For AM-AM curve, you can click on the Normalized check box
to choose whether to display the normalized results.
You can double-click the result window to enlarge it to see more detailed information and then double click again to be back to the default layout (3x2).
If Digital Predistortion is set to On, two curves will be displayed, with DPD and without DPD.
If Digital Predistortion is set to Off, only one curve will be displayed.