Waveform

This block provides Closedparameters for adding some basic processing to the original I/Q waveform file prior to further CFR/DPD/ET processing.

Calibrate Button

Opens a ClosedCalibration window where you can configure and then run the calibration algorithm.

See also Correction Filter and Correction Filter File.

Tools Button

Opens a Closeddrop-down menu with the following MATLAB tools. Waveform Type must be set to User-defined for the selections to be active.

Waveform Parameters

1. Basic

2. Processing

3. Burst Formation and Mask

4. Markers

Waveform Type

Waveform Location

I/Q Variable Name

File Type

File Name

Sample Rate

Waveform Length

Bandwidth

Resampling Ratio

Resampled Waveform Length

Filter

State

Maximum Order

Pass Frequency

Stop Frequency

Pass Ripple

Stop Ripple

Correction Filter

Correction Filter File

Burst Shape & Mask

Duty Cycle (%)

T1 (Lead Interval)

T2 (Waveform Interval)

T3 (Lag Interval)

T4 (Idle Interval)

Marker 1 Source

Marker 2 Source

Marker 3 Source

Marker 4 Source

1. Basic

Waveform Type

Choice: Preloaded | Signal Studio | User-defined | MATLAB Variable

Default: Signal Studio

Specify the type of waveform. It has three different choices, Preloaded, Signal Studio and User-defined.

Waveform Location

Choice: PC | RF Signal Generator

Default: PC

Coupling: This cell is grayed out if the waveform type is set to Preloaded or User-defined or when the RF Signal Generator Configuration is set to AWG + Signal Generator.

Select the waveform location for a signal studio waveform.

I/Q Variable Name

When MATLAB Variable is selected as the Waveform Type, clicking this parameter opens a Closedwindow where you can choose an I/Q variable name from the MATLAB workspace. The I/Q variable should be a 1-d complex array. If you have a valid license, you can launch MATLAB from the Signal Studio software's System menu and then use this window to browse or directly input a variable.

File Type

Choice: CSV/Text | Big Endian 16 Bits | MATLAB

Default: CSV/Text

Coupling: Available when the Waveform Type is set to User-defined.

Specify the format of the source file when the Waveform Type is set to User-defined.

File Name

Click the in the right side of the cell to browse the computer and select the waveform file.

Sample Rate

Range: 1 MHz to 8 GHz

Default: 5 MHz

Coupling: This cell is read-only when the Waveform Type is set to Predefined or Signal Studio.

It indicates the sample rate used by the waveform when Waveform Type is set to Predefined or Signal Studio. Sample rate is extracted from the header file of the waveform. You need to specify the sample rate manually when the Waveform Type is set to User-defined.

Waveform Length

Waveform Length is read-only and it indicates the sample number in the waveform.

Bandwidth

Range: 1 to 200 MHz

Default: 5 MHz

Specify the bandwidth of the waveform.

2. Processing

Resampling Ratio

Range: 0.1 to 20

Default: 1

Coupling: The resultant sampling rate will not be greater than 200 MHz if the configuration is set to RF Signal Generator (MXG-B). The resampling ratio is displayed as a fraction after rational approximation. You should set a proper resampling ratio to make the resampled waveform cyclic, that is, the waveform length should be able to be divided by the decimator. The software doesn’t do extra coupling to make sure the waveform is cyclic, instead, it reports an error after you click Run when the waveform length cannot be divided by the decimator.

Specifies the resampling ratio (RSR) that up-samples the waveform. This is not the RSR used by the imported waveform. Rather, it is the RSR that the software uses to resample the waveform. It is expected that the signal employed to extract a DPD model should have a resampling rate no less than 3. If the selected waveform's up-sampling ratio is less, it can be up-sampled here with a resampling ratio greater than 3. If the user-defined or chosen waveform file already has a high over-sampling ratio beyond the capability of the selected signal generator, then the created waveform must be be resampled with a ratio less than 1.

Resampled Waveform Length

Range: 1 to Int32.Max

Default: 10000

Coupling: It equals the product of Waveform Length and Resampling Ratio.

It indicates the sample number of the waveform after resampling.

Filter

Set the parameters to design a Parks-McClellan low pass filter in the menu below. The Parks-McClellan design method uses the Remez exchange algorithm to design linear phase FIR filters such that a filter has minimum weighted Chebyshev error in approximating a desired ideal frequency response. For more details, refer to Chapter 7.4.3 in "The Parks-McClellan Algorithm in Discrete-Time Signal Processing, 2nd ed".

The filter can be depicted as below, in which

fp is the pass frequency,

fs is the stop frequency,

δp is the pass ripple,

δs is the stop ripple.

 

Sate

Choice: On | Off

Default: Off

Double-click or use the drop-down menu to enable or disable the application of the filter.

Maximum Order

Range: 1 to 2048

Default: 300

Set the maximum filter length. The filter’s length is clipped to the Maximum Order if the minimum filter length required to satisfy its specification exceeds the Maximum Order.

Pass Frequency

Range: 1 Hz to (Stop Frequency - 0.0015*Sample Rate*Resampling Ratio in Waveform block/2)

Default: 1.25 MHz

Set the pass frequency of the filter.

Stop Frequency

Range: 2 Hz to (0.5*Sample Rate*Resampling Ratio)

Default: 1.5625 MHz

Set the stop frequency of the filter.

Pass Ripple

Range: 0.0001 to 5.0

Default: 0.01

Set the maximum ripple in the pass band.

Stop Ripple

Range: 6.0 to 200.0

Default: 50.0

Set the maximum ripple in the stop band.

Correction Filter

Choice: On | Off

Default: Off

This value indicates whether the correction filter will be applied when you run the test flow.

See also Calibrate Button and Correction Filter File.

Correction Filter File

Default: C:\Work\ChannelResponse.csv

Specifies the correction filter file name. When you click the ClosedCalibrate button the correction filter coefficients are saved to this file. When Correction Filter is on, the filter coefficients will be read from the file and used in the test flow.

See also Calibrate Button.

3. Burst Formation and Mask

Burst Shape & Mask

Choice: On | Off

Default: Off

Coupling: Its state is mutually exclusive with the state of Envelope Tracking. They can’t be set to On at the same time.

Enable or disable the construction of burst by adding intervals to the waveform and generating of a PA enabling mask signal. When it is set to on, intervals will be added prior to and after the waveform to achieve a certain duty cycle. In the meantime, a mask signal is generated according to the specified time intervals.

Duty Cycle (%)

Range: 1% to 100%

Coupling: Available when Burst Shape & Mask is set to On. Its value is equal to T2/(T1+T2+T3+T4)*100%.

It indicates the Duty Cycle of the burst.

T1 (Lead Interval)

Range: 0 to 100 μs

Default: 1 μs

Coupling: Available when Burst Shape & Mask is set to On. It should be less than T4.

Specifies the time interval ahead of waveform.

T2 (Waveform Interval)

Range: 1 μs to 10 s

Default: 2 ms

Coupling: Available when Burst Shape & Mask is set to On. It equals to the quotient of the Waveform Length and the Sample Rate.

It indicates the time length of the waveform.

T3 (Lag Interval)

Range: 0 to 10 μs

Default: 1 μs

Coupling: Available when Burst Shape & Mask is set to On.

Specify the time interval after waveform.

T4 (Idle Interval)

Range: 0 to 60 s

Default: 1 ms

Coupling: Available when Burst Shape & Mask is set to On.

Specifies the length of the idle interval added to the waveform.

4. Marker

Marker 1 Source

Configure the marker points for Marker 1 using the Marker Source Selection dialog box.

The signal generator outputs the Marker 1 signal from the rear-panel EVENT 1 output. For more information, see the signal generator's User Guide.

Marker 2 Source

Configure the marker points for Marker 2 using the Marker Source Selection dialog box.

The signal generator outputs the Marker 2 signal from the rear-panel EVENT 2 output. For more information, see the signal generator's User Guide.

Marker 3 Source

This parameter is read-only and it indicates Marker 3 is used to control ALC hold.

The signal generator outputs the Marker 3 signal from the rear-panel EVENT 3 output. For more information, see the signal generator's User Guide.

Marker 4 Source

This parameter is read-only and it indicates Marker 4 is used to control Pulse/RF Blank.

The signal generator outputs the Marker 4 signal from the rear-panel EVENT 4 output. For more information, see the signal generator's User Guide.