Waveform (Dual-band PA Test)

This block is to load the original IQ waveform file with some basic processing, then pass it along to do further CFR/DPD processing.

1. Basic

2. Processing

3. Markers

Waveform Type

File Type

File Name

Sample Rate

Waveform Length

Time Duration

Bandwidth

Resampling Ratio

Resampled Waveform Length

Filter

State

Maximum Order

Pass Frequency

Stop Frequency

Pass Ripple

Stop Ripple

Marker 1 Source

Marker 2 Source

Marker 3 Source

Marker 4 Source

1. Basic

Waveform Type

Choice: Preloaded | Signal Studio | User-defined

Default: Signal Studio

Specify the type of waveform. It has three different choices, Preloaded, Signal Studio and User-defined.

File Type

Choice: CSV/Text | Big Endian 16 Bits | MATLAB

Default: CSV/Text

Coupling: Available when the Waveform Type is set to User-defined.

Specify the format of the source file when the Waveform Type is set to User-defined.

File Name

Click the in the right side of the cell to browse the computer and select the waveform file.

Sample Rate

Range: 1 MHz to 8 GHz

Default: 5 MHz

Coupling: This cell is read-only when the Waveform Type is set to Predefined or Signal Studio.

It indicates the sample rate used by the waveform when Waveform Type is set to Predefined or Signal Studio. Sample rate is extracted from the header file of the waveform. You need to specify the sample rate manually when the Waveform Type is set to User-defined.

Waveform Length

Waveform Length is read-only and it indicates the sample number in the waveform.

Time Duration

Time Duration is read-only and it indicates the time duration of the selected waveform.

Bandwidth

Range: 1 to 200 MHz

Default: 5 MHz

Specify the bandwidth of the waveform.

2.Processing

Resampling Ratio

Coupling: It equals to the ratio of Sample Rate in Digital Predistortion model to Sample Rate in Waveform model.

Resampling Ratio is read-only and it indicates the oversampling ratio to be applied on the selected waveform.

Resampled Waveform Length

Coupling: It equals to the multiplication of the Waveform Length and the Resampling Ratio.

It is read-only and indicates the sample number of the waveform after oversampling.

Filter

Set the parameters to design a Parks-McClellan low pass filter in the menu below. The Parks-McClellan design method uses the Remez exchange algorithm to design linear phase FIR filters such that a filter has minimum weighted Chebyshev error in approximating a desired ideal frequency response. For more details, refer to Chapter 7.4.3 in "The Parks-McClellan Algorithm in Discrete-Time Signal Processing, 2nd ed".

The filter can be depicted as below, in which

fp is the pass frequency,

fs is the stop frequency,

δp is the pass ripple,

δs is the stop ripple.

 

Sate

Choice: On | Off

Default: Off

Double-click or use the drop-down menu to enable or disable the application of the filter.

Maximum Order

Range: 1 to 2048

Default: 300

Set the maximum filter length. The filter’s length is clipped to the Maximum Order if the minimum filter length required to satisfy its specification exceeds the Maximum Order.

Pass Frequency

Range: 1 Hz to (Stop Frequency - 0.0015*Sample Rate*Resampling Ratio in Waveform block/2)

Default: 1.25 MHz

Set the pass frequency of the filter.

Stop Frequency

Range: 2 Hz to (0.5*Sample Rate*Resampling Ratio)

Default: 1.5625 MHz

Set the stop frequency of the filter.

Pass Ripple

Range: 0.0001 to 5.0

Default: 0.01

Set the maximum ripple in the pass band.

Stop Ripple

Range: 6.0 to 200.0

Default: 50.0

Set the maximum ripple in the stop band.

3. Marker

Marker 1 Source

Choice: None | FromWaveformFile | WaveformStart | UserDefined

Default: WaveformStart

Configure the marker points for Marker 1 using the Marker Source Selection dialog box.

The signal generator outputs the Marker 1 signal from the rear-panel EVENT 1 output. For more information, see the signal generator's User Guide.

Marker 2 Source

Configure the marker points for Marker 2 using the Marker Source Selection dialog box.

The signal generator outputs the Marker 2 signal from the rear-panel EVENT 2 output. For more information, see the signal generator's User Guide.

Marker 3 Source

Choice: RF ALC Control | UserDefined

Default: RF ALC Control

This parameter is editable only when the Waveform Type is User-defined.

This parameter indicates Marker 3 is used to control ALC hold.

The signal generator outputs the Marker 3 signal from the rear-panel EVENT 3 output. For more information, see the signal generator's User Guide.

Marker 4 Source

Choice: RF Blanking | UserDefined

Default: RF Blanking

This parameter is editable only when the Waveform Type is User-defined.

This parameter indicates Marker 4 is used to control Pulse/RF Blank.

The signal generator outputs the Marker 4 signal from the rear-panel EVENT 4 output. For more information, see the signal generator's User Guide.