To generate signals using the N7615C Signal Studio for Mobile WiMAX 2018 software, you must have a properly configured PC and a properly configured instrument, as described in the following table.
|
Instruments |
Requirements |
|---|---|
|
N5172B EXG X-Series RF vector signal generator |
Firmware:
Required options:
Recommended options:
|
|
N5182B MXG X-Series RF vector signal generator |
Firmware:
Required options:
Recommended options:
|
|
N5182A MXG vector signal generator |
Firmware:
One of the following baseband generator options:
One of the following frequency options:
Recommended options:
|
|
E4438C ESG vector signal generator |
Firmware:
One of the following baseband generator options:
One of the following frequency options:
Recommended options:
|
|
E8267D PSG vector signal generator |
Firmware:
Required options:
Option E8267D-UNW (narrow pulse modulation) is NOT recommended because it may degrade the EVM performance at 3.5 GHz or below. Option E8267D-UNU and E8267D-UNW are mutually exclusive. Recommended options:
|
|
vector signal analyzer (VSA): PSA-series, MXA, 89640A, or 89641A |
89601A VSA software with Option B7Y (802.16 OFDMA Modulation Analysis), recommend version 7.01 or later (Required to complete the tutorials) |
|
M9381A PXIe vector signal generator |
Driver:
|
|
Solutions |
Instruments |
Requirements |
|---|---|---|
|
(Two signal generators driven from 10 MHz reference and the same trigger) |
Two E4438C ESGs -or- Two E8267D PSGs |
E4438C ESGs:
E8267D PSGs:
|
|
(Two signal generators with baseband generator clock coherence, but without RF common LO) |
Two N5182A MXGs -or- Two E4438C ESGs -or- Two E8267D PSGs |
N5182A MXGs:
E4438C ESGs:
E8267D PSGs:
|
|
One external ARB clock |
Working with E4438C or E8267D;
|
|
|
(Two signal generators with RF common LO and baseband generator clock coherence) |
Two N5182A MXGs -or- Two E4438C ESGs -or- Two E8267D PSGs |
N5182A MXGs:
E4438C ESGs:
E8267D PSGs:
|
|
Lock box plus external ARB clock or amplifier distribution |
Working with E4438C ESG:
Working with E8267D PSG:
|
200 GB HDD with 2 GB free disk space at runtime (5 GB or higher recommended)
1024 x 768 screen resolution (1280 x 1024 recommended)
If you use a high-resolution display, the GUI's font size may appear too small to read. To resolve this, lower your PC's display resolution, but make sure the display scaling remains set at 100 percent, otherwise portions of the GUI will become truncated and hidden from view.
Windows 10 (64 bit):
1 GHz or faster
2 GB of memory minimum
1.5 GB hard disk space (includes 1 GB for Microsoft .NET Framework and 65 MB for the Keysight IO Libraries)
Microsoft Internet Explorer 11.0 or later
128 MB graphics memory with DirectX 9 graphics support (recommended)
Windows 7 (64 bit):
1 GHz or faster
2 GB of memory minimum
1.5 GB hard disk space (includes 1 GB for Microsoft .NET Framework and 65 MB for the Keysight IO Libraries)
Microsoft Internet Explorer 11.0 or later
128 MB graphics memory with DirectX 9 graphics support (recommended)
Microsoft .NET Framework 4.5.2 or later
Keysight IO Libraries, version 18.0 or later
Keysight License Manager 5 (4. Downloading and Installing Keysight License Manager 5)
Keysight License Service (included with installer)
Keysight Host Processor Platform (included with installer)
Installed GPIB IO interface card, LAN interface card, or USB/GPIB interface connector
Keysight VISA
Microsoft Windows Installer version 2.0 or later
WiMAX and Mobile WiMAX are US trademarks of the WiMAX Forum.