In this example, you will use the N7615C software to create a waveform that contains 3 "basic" carriers for WiBro. You might use this type of setup for designing and manufacturing power amplifiers and repeaters.
The N7615C software has predefined configurations for the 3FA and 6FA WiBro signals, so this example focuses on helping you learn how to use the software.
From the Welcome dialog, select
Click in the navigation tree on the left. Set the instrument's frequency to 2.345 GHz and leave the amplitude at the default value of –10 dBm.
Click in the navigation tree on the left.
The table at the top shows the default setup with a single carrier. The type of carrier depends on whether the software is set up to connect to an instrument that has a license for basic or advanced capability. The buttons above the table allow you to access the predefined configurations, add a basic or advanced mode carrier, delete a carrier, or copy a carrier.
Click the
button to see the predefined configurations
that are available, then click cancel to return to the Waveform Setup.
If the table shows an advanced carrier, click the
button to delete it and then click
to add a basic OFDMA carrier.
Change to 63.952%. This is the default for WiBro.
Click on in the table or in the navigation tree on the left to access more signal parameters. is available on this window. Change the value to 8.75 MHz. The value of will update to 8/7.
Click in the tree view to view the available parameters.
Click on and note the simple setup window for the zone. The frame graph is displayed at the bottom of the window. In a basic carrier, you cannot configure bursts so there is no zone-level view. Change to 64QAM and to 26.
The MAC PDU table at the bottom of the window allows you to configure the MAC PDU. Click and see the Data Source Selection window to choose the Data Type. You can choose S(QPSK), S(16QAM), S(64QAM), PN 9, PN 15 or User Defined Bits to input any desired data. For this example, leave the Data Type at the default choice of PN9. You have completed the carrier configuration.
Click
and then click the button twice to add 2 carriers with the same configuration.
Click and change the to -9 MHz.
Click and change the to 9 MHz.
This completes the basic setup of the 3FA signal.
Click
and then click the
button in the toolbar. You will see the CCDF graph
for the waveform (all 3 carriers). Note that the
default view is now the Burst CCDF, although Waveform CCDF is still available.
The CCDF for each individual carrier can be viewed by clicking on that
carrier in the navigation tree. Click
here
for more information.
Click , select the tab near the bottom of the window, and use the drop down arrow to view the power, I/Q, and spectrum plots for the waveform.
Click the tab.
The yellow line shows the relative power for the waveform, and you can see the relative amplitude levels for different symbols by moving the mouse over a portion of the downlink burst. The dark red portion shows the symbols that are used as the power reference for the instrument. By default, the software turns marker 4 on during these symbols (see marker settings on Waveform Setup page), and marker 4 is used to control the ALC hold function in the instrument (as shown in Instrument setup page, under ). These are the symbols where the instrument's ALC will be active, so the power level of these symbols will be equal to the instrument's amplitude setting.
You can choose to change the power reference by clicking on a different set of symbols. When you do this, the new symbols will be shown in dark red. When you move the mouse over that section, it will be shown as amplitude = 0 dB and the levels elsewhere in the waveform will be relative to that value. The new amplitude offset value will be displayed in the Waveform Setup parameter table above the graph, as ALC Reference Offset under . The power level of these selected symbols will now be equal to the instrument's amplitude setting.
Click the
button in the toolbar to download the waveform
to the instrument. On the spectrum analyzer, use the band power markers
to measure the power level in each carrier. What
do you observe about the power levels?
The relative power level for each carrier can be adjusted by clicking on the node and changing the power setting. This allows you to compensate for any flatness imperfections in the instrument.
If desired, set up the 89601A software to demodulate the signal and measure the EVM.
Some important notes:
You can import *.xml setup files from the N7615A into the N7615C by changing the file type selection when you open a settings file. However, the *.scp setup files cannot be used with N7615A version 1.2.2.0 or earlier.
The VSA can only demodulate a single carrier. Therefore, the demodulation analysis data that you see is only for the carrier at the center frequency.