3. DCD Settings

In this version of Signal Studio for Mobile WiMAX, DCD and UCD are transferred in different bursts from DL-MAP and UL-MAP, so they have their own burst allocations. The properties of these burst settings are exactly the same as those in a normal downlink burst.

Include DCD Message

Choices: On, Off

Select the use of DCD Message MAC PDU in the DL-MAP burst.

DCD CID

Range: 0 to FFFF

Set the CID for the DCD in hex. This parameter is shared with UCD CID and is configurable when Include DCD Message is On and Auto DL-MAP is Normal.

DIUC Generation Type

Use the drop-down menu or double-click to automatically generate the DIUC table or not.

DIUC 0 through DIUC 12

Use the drop-down menu or double-click to specify the mapping table of the DIUC. This is configurable when Auto DL-MAP is either Normal or Compressed, and DIUC Generation Type is Manual.