Go to topic

6. Dual ARB Marker Utilities

Pulse/RF Blanking

Choice: None | Marker 1–4

Default: None

Use this cell after downloading and synchronizing with the instrument.

Double-click or use the drop-down menu to select an RF blanking function.

The software uses Marker3 to control the RF blanking and Marker4 for ALC settings. These settings should NOT be changed unless you are knowledgeable of how the changes will affect the waveform playback. See also Marker1-4 in Project Property.

ALC Hold

Choice: None | Marker 1–4

Default: None

Use this cell after downloading and synchronizing with the instrument.

Double-click or use the drop-down menu to select a marker for ALC hold. Use ALC hold when you have a waveform signal that has idle periods, or when the increased dynamic range with RF blanking is not desired.

Alternate Amplitude

Choice: None | Marker 1–4

Default: None

Use this cell after downloading and synchronizing with the instrument.

Double-click or use the drop-down menu to select a marker for enabling the alternate amplitude function.

Configure the alternate amplitude parameters from the Amplitude hardkey menu of the instrument.

For more information about alternate amplitude and marker settings, refer to the instrument's user's guide.

This parameter is not available with all instrument model numbers and may be grayed out.

Marker1–4 Polarity

Choice: Positive | Negative

Default: Positive

Use this cell after downloading and synchronizing with the instrument.

Double-click or use the drop-down menu to select the active polarity for Marker 1–4.