HARQ Sub-Burst# (IR CC)

The figure above shows the definition of HARQ burst allocation. Each sub-burst size is indicated by the "Duration” property and slots are allocated in frequency-first order from the end of last sub-burst. For the last sub-burst, if assigned slots are larger than occupied slots, 0xff will be padded to make the data block fit the assigned slots size.

At least one MAC PDU is defined in the HARQ sub-burst, otherwise, an error will be displayed on status bar. You can add, delete, copy or change the order of MAC PDUs. To generate a sub-burst, ccitt-16 bit CRC is appended to the concatenated MAC PDUs after padding and then channel coding is applied to the data block.

When allocated in a non-STC zone, the parameters for IR CC HARQ Sub-burst are:  

When allocated in an STC zone, the parameters for IR CC HARQ Sub-burst are:

1. Sub-burst Settings

Basic CID

Range: 0 to 65535

Enter the Basic Connection ID that indicates a specific subscriber station where the HARQ DL MAP IE are described for.

DIUC Indicator

Choices: On, Off

Enable or Disable the DIUC (Downlink Interval Usage Code) indicator that Indicates whether the DIUC and Repetition will be included in the HARQ DL MAP IE.

When DIUC Indicator is set to off, the modulation and coding and Repetition Coding are disabled.

DIUC Indicator of the first sub-burst in the list must be set to ’r;true’. Otherwise, an error message will be displayed on the status bar.

Modulation and Coding

Select the modulation type, coding type, and coding rate from the drop down menu. The type of coding available depends on the burst profile.

Repetition Coding

Choices: None, 2, 4, 6

Select the number of times the coded or uncoded data is repeated.

Repetition number of 2 4 6 can only be applied when the Modulation type is QPSK. Otherwise, an error message displays in the status bar.

Duration [Slots]

Displays how many slots are needed for the HARQ sub-burst based on the total length of sub-burst after CRC calculation. The value of this parameter should be the least number of slots that can accommodate "Sub-burst length” + 16 bits "CRC” data. Padding bits is appended before CRC when the allocation is larger than needed.

2. HARQ Settings

ACID

Range: 0 to 15

Enter the ARQ Channel ID that indicates a specific HARQ transmission between a base station and subscriber station. This is used in the HARQ MAP IE.

AI_SN

Range: 0 to 1

Enter the AI_SN (ARQ Identifier Sequence Number) value of a specific HARQ transmission. When the AI_SN field in the HARQ channel remains the same between two HARQ burst allocations, the sub-burst is retransmitted. This is used in the HARQ MAP IE.

ACK Disable

Choices: On, Off

Select the ACK Disable status that indicates whether the allocated sub-burst requires an ACK to be transmitted by subscriber station. This is used in the HARQ MAP IE. This parameter determines the number of ACK channels.

SPID Sequence

Range: 0 to 3

Enter the sequence string of subpacket IDs, using comma(',') as the separator. This sequence will be automatically repeated or truncated depending on the number of build frames. 

For example, sequence '0,1,2,3' indicates all the four SPIDs will be used in generating multi-frame waveform.

3. CQI Control Settings

CQI Control

Choices: On, Off

Select the state of CQI Control that indicates whether CQI Control information will be included in the HARQ DL MAP IE.

Only when this parameter is set to On, Duration(d) becomes configurable.

Only when CQI Control is set to On and Duration(d) is set to none zero, Allocation Index, Period(p) and Frame Offset become configurable.

Duration (d)

Range: 0 to 15

Enter the duration value d that indicates a CQI feedback is transmitted on the CQI channels by the subscriber station for 2^(d-1) frames. This is used in the HARQ DL MAP IE.

When Duration (d) is set to 0, Allocation Index, Period (p) and Frame Offset are disabled and grayed.

Allocation Index

Range: 0 to 63

Enter the index of the channel in a frame the CQI report should be transmitted by the subscriber station. This is used in the HARQ DL MAP IE.

Period (p)

Range: 0 to 7

Enter the period value p that indicates a CQI feedback is transmitted on the CQI channels indexed by the (Allocation Index) by the subscriber station in every 2^p frames. This is used in the HARQ DL MAP IE.

Frame Offset

Range: 0 to 7

Enter the frame offset value that indicates subscriber station starts reporting at the frame of which the number has the same 3 LSB as the specified frame offset. This is used in the HARQ DL MAP IE.

4. Dedicated DL Control Settings

Dedicated DL Control

Choices: On, Off

Select the state of Dedicated DL Control that indicates whether the Dedicated DL control information will be included in HARQ DL MAP IE.

Number of SDMA Layers

Range: 0 to 3

Enter the total number of SDMA (spatial division multiple access) layers associated with HARQ MAP IE when Dedicated DL Control is set to On.

4. Dedicated MIMO DL Control Settings

Dedicated MIMO DL Control

Choices: On, Off

Select the state of Dedicated MIMO DL Control that indicates whether the Dedicated MIMO DL control information will be included in HARQ DL MAP IE.

Matrix

Choices: Matrix A, Matrix B

Select the transmission matrix indicator.