Clicking Instrument in the
tree view
displays the Instrument Settings table in the node view of the main window.
The figure below shows the Instrument node for a signal generator connection. Click a button or click an item in the Instrument Control list for information on that button or item.
Click the plus
box to expand the table and access those
parameters.
Press this button
to send the software parameters to the connected instrument.
Press this button
to retrieve the parameters from the connected instrument.
Press this button
to deactivate remote operation and return the instrument to local (front
panel) control.
Press this button
to set the instrument to a known state, either factory-defined
or user-defined.
Refer to the instrument's user's guide for information on setting a user-defined state.
Press this button
to execute an I/Q DC Calibration to minimize errors associated with offset
voltages.
DC Cal minimizes I/Q offset errors for a single frequency only, and must be repeated if the instrument's settings change.
Download a waveform to set the correct parameters for the target instrument, and make this button available.
Press this button
to execute a manual power search calibration.
This is an internal calibration routine that improves output power accuracy when ALC is off. A power search is recommended for pulse-modulated signals with pulse-widths less than two microseconds.
Download a waveform to set the correct parameters for the target instrument, and set ALC to Off to make this button available.