In this example, you will set up an uplink signal with ranging bursts and make measurements on that uplink signal with the 89601A.
In Signal Studio, select
> from the menu or click
the
button in the toolbar to start a new waveform configuration.
Leave the instrument settings at the default frequency
of 1 GHz and amplitude of –10
dBm.
Click in the navigation tree and change to Uplink Only (TDD).
Click on and change the bandwidth to 5 MHz and FFT size to 512.
Click on Uplink in the navigation tree.
Change to 9. Note that this panel has a section titled "Other Region Settings” that summarizes the settings for the fast feedback, ACK region, initial ranging, and periodic ranging regions. Click on "+” next to each heading to show more details of the settings.
Click in the navigation tree on the left. On the right, change to on to create the region. The number of subchannels for the initial ranging region is a multiple of 6, and the number of symbols is a multiple of 2.
Change to 4. Ranging regions are usually placed in the upper left portion of the zone at the beginning of the UL-PUSC region, but this is not a requirement.
Note the message in the status bar stating the initial ranging zone doesn’t satisfy slot boundary. This is because UL-PUSC slots are 3 symbols wide but the 4 symbols in the initial ranging region does not match one of those boundaries. We will take care of this later.
Click
to add 2 ranging bursts. Give
each burst a code number (0 to 255) and a slot location (0 or 1). Note
that ranging bursts are allowed to overlap. This would be the case if
multiple subscriber stations are trying to send initial ranging signals
to the base station at the same time. The base station distinguishes the
signals by the unique code number, similar to CDMA.
Click Uplink to view the zone layout. Notice that the 2 symbols that form the rest of the slot boundary for the initial ranging region are crossed out, and user Burst #1 starts on the next slot boundary. We can solve the slot boundary problem either by increasing the size of the initial ranging region, or adding a periodic ranging region. Both types of ranging regions are combined when aligning to slot boundaries. We will choose the second method.
Click on the left, and on the right panel, change to on and set to 2 and to 4.
Add some ranging bursts and assign a code number and slot location to each.
Click Uplink and note that the periodic ranging region has satisfied the slot boundary so the symbols with the red cross marks are gone. Add another regular data burst.
Click on , change the to 50 bytes.
Click , change to 16QAM (CC) 1/2, to 150 bytes. Note how the bursts wrap around the ranging region. Generate and download the waveform.
In the 89601A VSA software, go to > > .
Configure the proper center frequency, span, and range to measure the instrument's signal.
Go to > > > to turn on the demodulator.
Go to > .
On the Format tab, select , click on and select .
Next we configure the VSA to measure the UL-PUSC zone. Select the Zone Definition tab and click on the Edit Active Zone button.
Set PermBase to 0 and Length to 9 symbols.
The VSA does not actually analyze ranging regions, so it can only measure the user bursts. To get the bursts to wrap properly, we still need to configure the ranging region. Delete any existing bursts.
Click , then change Burst Shape to rectangular and select Burst Type of CDMA.
Configure this burst to include the entire ranging region of 6 symbols by 6 subchannels. This burst will have diagonal lines drawn through it to indicate that it is a special burst, and VSA software will not provide the usual measurements for it such as the constellation or OFDM Syms/Errs. However, you can set the Trace Data type to OFDM Data Burst Info, and the VSA will display the detected CDMA ranging codes along with the power levels, length in symbols, and location (subchannel and symbol)
Add the two user bursts, selecting the appropriate modulation type and checking the Active box for each burst. Make sure Burst Shape is set to wrapped and Burst Type is normal. When you’re done editing, click to exit and make sure the Data Burst Analysis box is checked on the Zone Definition tab and measure the data bursts.