This example shows you how to set up the new zone types that have been added to the N7615C, and how to set up the 89601A VSA software to demodulate these new zones.
In version 7.01 or later of the 89601A option B7Y VSA software, the VSA has the ability to automatically decode a DL-MAP and set up the zone maps for demodulating a signal. Since the signal created in Part 1 contains a DL-MAP (with the added step), we can either use the auto DL-MAP decoding or manually set up the demodulation. For tutorial purposes, we will set up the demodulation manually first, then show how to use the auto DL-MAP decoding.
Select
> from the menu or click
the
button in the toolbar to start a new waveform configuration.
Click I in the navigation tree on the left. Set the instrumentr's frequency to 2.5 GHz and leave the amplitude at the default value of –10 dBm.
Click in the navigation tree. The carrier table should show one advanced carrier. If not, delete the basic carrier and add an advanced carrier. We will use the default Waveform Setup parameters shown on this page.
Click and change the to 5 MHz and to 512.
Click
in the navigation tree. Click the
button above the zone table and add an AMC
zone. Signal Studio supports 2x3 AMC zones, which refers to a basic structure
of 2 bins x 3 symbols, where a bin is 9 adjacent subcarriers. Note that
you cannot have just an AMC zone in the downlink, because the first zone
is required to be a DL-PUSC zone.
Increase the number of symbols in the AMC zone to 9. (Note this value must be a multiple of 3 because the AMC 2x3 slot size is 3 symbols long.)
Click to view the settings for this zone. Click on the burst that has been added by default and delete it by clicking on the "X" button. In section 3 of the parameter table, set "Auto DL-MAP" to Normal. You should now have 2 symbols in this zone, containing an FCH and DL-MAP.
Click
to view the settings for this zone. As with any downlink zone except the
first DL-PUSC zone, you can set the Permutation Base and PRBS ID. Check
the
box for more description of these fields. There
is also a field for turning dedicated pilots on or off. When
dedicated pilots are on, it indicates that a subscriber station should
only use the pilots specific to its burst for channel estimation. For
now, leave this field set to off.
Set to off. Add a burst with 16QAM (CC) 3/4 modulation and another burst with 64QAM (CC) 2/3 modulation for a total of 3 bursts in the zone.
Double-click on the row with the first burst, or click on in the navigation tree to display the configuration for the burst. Change the to 110 bytes and change the to 20.
Click in the navigation tree and make the following changes:
to 3
to 6
to 10
to 0
to 170 bytes
Click in the navigation tree and make the following changes:
to 3
to 6
to 14
to 10
to 310
Click the
button in the toolbar to verify that there
are no errors with the setup. Error messages are
also displayed at the bottom of the window in the status bar. Click the
button to download the waveform into the instrument.
Start the 89601A VSA software and go to > > . Configure the proper center frequency, span, and range to measure the signal from the instrument.
Go to > > > to turn on the demodulator.
Go to > . On the Format tab, click on and select .
Next we configure the VSA to measure the AMC zone. Select the Zone Definition tab and click on the Edit Active Zone button. For Type, select AMC. The AMC settings will be displayed. The default is "2:3” which is the 2x3 zone configured in Signal Studio, so no change is needed. The Offset should be set to 3 symbols (to skip the preamble and 2 symbols of DL-PUSC zone in the downlink signal). Length should be set to 9 symbols. Change the PRBS ID to 0, delete the default FCH burst, and add the data bursts that you set up in Signal Studio in the AMC zone.
Return to the Zone Definition page. Check the box for Data Burst Analysis if needed to make the measurement on the bursts in the AMC zone.
Try measuring one burst at a time. Notice that in the Error Vector Spectrum plot, all subcarriers for a burst are adjacent to each other. Also note the burst power profile in the Search Time display.
In Signal Studio, click on Zone #2, AMC in the navigation tree. On the right top panel, change Dedicated Pilots to on and then generate and download the waveform. In the VSA software, go to the Demodulation Properties window, Zone Definition tab, and click the Edit Active Zone button, and check the box for Dedicated Pilots on the left, then click OK. What is the impact of this on the VSA measurement?
You should see that the spectrum has changed and the in-band power is lower. In the Search Time display, you should see a big power drop out corresponding to the symbols where there is no data. In the Error Vector Spectrum display, you should see that there are now no pilots present for the subcarriers where there is no data. Turning dedicated pilots on causes Signal Studio to do 2 things: 1) only transmit pilots for the subchannels that contain burst data, and 2) change the Zone IE in the DL-MAP to indicate dedicated pilots mode, to indicate that a subscriber station should only use the pilots specific to its burst for channel estimation. In normal mode, pilots are transmitted even when there is no data being transmitted for a particular symbol. With dedicated pilots turned on, the source does not transmit anything when there is no data, so the result is the power dropout during the middle 3 symbols of the DL-AMC zone.
Dedicated pilots are used in systems with beamforming.
Now we will use the automatic DL-MAP decoding feature in the VSA to make the same measurement. Repeat steps 1 through 3 to preset the demodulation setup and input the basic format parameters.
In the Demodulation Properties window, click on the Advanced tab and uncheck the box next to "Decode ULMAP” since there is no UL-MAP present in this signal.
Click on the Zone Definition tab, and select "Auto”. After one or two updates, you should see the zone maps displayed. Click on the second zone to measure the AMC zone. To measure a single burst only, select "Use Map File” and then click on the desired burst.
In Signal Studio, select
> from the menu or click
the
button in the toolbar to start a new waveform configuration.
Leave the instrument settings at the default frequency
of 1 GHz and amplitude of –10
dBm.
Click in the navigation tree and change to Uplink Only (TDD).
Click Uplink in the navigation tree. Change to off, then change to 9.
Add a second regular burst to the zone.
Click and change the to 250 bytes.
Click , change to 16QAM (CC) 3/4, and change to 450 bytes.
Generate and download the waveform.
In the 89601A VSA software, go to > > . Configure the proper center frequency, span, and range to measure the instrument's signal. Go to > > > to turn on the demodulator.
Go to > . On the Format tab, select , click on and select .
Next we configure the VSA to measure the PUSC zone. Select the Zone Definition tab and click on the Edit Active Zone button. Set the PermBase to 0 and Length to 9 symbols. Uncheck the box. Delete any existing bursts before creating the new ones. Create the two bursts that you set up in Signal Studio: Burst 1 is QPSK, 44 slots, Burst 2 is 16QAM, 26 slots. If needed, set to Wrapped.
Return to the Zone Definition page. Check the box for Data Burst Analysis if needed to make the measurement on the bursts in the PUSC zone.
Notice there is a dot in the center of the constellation, and the OFDM Error Vector Spectrum plot shows green data points in addition to the orange and red ones that correspond to the two data bursts. Why is this?
(Answer: Look on the Advanced tab in Demod Properties on the VSA. Note that the default settings say "include inactive subchannels.” Uncheck this box and notice that the center dot and green data points disappear. The default includes inactive subchannels because of the way RCE/EVM is defined for uplink signals.)