Carrier n Setup

Carrier Configuration Summary Table

This table enables you to view the key parameters for each carrier in the waveform. You can also add or delete carriers using the buttons above the table (see descriptions below). Double-clicking a carrier row activates the setup tables for that carrier. You can use a maximum of 16 carriers.

This button opens a window of Closedpre-defined carrier configuration selections. Double-clicking a configuration replaces the current configuration in the setup table.

This button opens a Closeddrop-down menu for selecting a carrier to add to the setup table. The carrier is inserted at the bottom of the list in the setup table.

This button deletes the currently highlighted carriers in the setup table. You can highlight multiple carriers by holding down the CTRL key while selecting the carriers. You can also use the SHIFT key to select a succession (group) of carriers.

This button copies the currently selected carrier and adds it to the bottom of the list in the summary table.

An asterisk shown with a carrier entry indicates that the parameters of a channel for that carrier have changed. 

Signal Studio for Mobile WiMAX does not allow you to create multi-carrier signals when you select the multiple antennae configuration, due to the complexity and incompatibilities that could result from having different carriers with different STC/MIMO configurations.