1. Open the setting file with Notepad or Xml Editor and move to hardware configuration part (see below). "Source_IntArb_HwSystem" indicates it was created for M x 1(For
Signal Generator) hardware system.
<Current System>
<Function>Single Antenna</Function>
<Source_IntArb_HwSystem>
<Name><Simulated Hardware></Name>
</Source_IntArb_HwSystem>
</CurrentSystem>
2. If user wants to reuse it in another hardware system, for example 1 Ant Tx(for PXB), replace hardware type "Source_IntArb_HwSystem" with
"Source_N5106_HwSystem" (hardware system type for 1 Ant Tx (for PXB), see mapping table below).
<CurrentSystem>
<Function> Single Antenna</Function>
<Source_N5106_HwSystem>
<Name><Simulated Hardware></Name>
</Source_N5106_HwSystem>
</CurrentSystem>
Then seek to the <SgModel> part, change the target instrument type to "N5106A" (target instrument type for 1 Ant Tx(for PXB), see mapping table below). Note that for
Mx2 or MIMO case, two occurrences of <TargetInst> shall be replaced.
<SigGen>
<SgModel>
<TargetInst>N5106A</TargetInst>
3. Save the setting file and then open it in Signal Studio, user can get the original waveform setup with the new hardware system.
Here is the mapping table between Quick Setup, Hardware System, Target Instrument and Function.
|
Function |
Quick Setup |
Hardware System |
Target Instrument |
|---|---|---|---|
|
Single Antenna |
Mx1 (for Signal Generator) |
Source_IntArb_HwSystem |
E4438C/N5182A |
|
1 Ant Tx (for PXB) |
Source_N5106_HwSystem |
N5106A |
|
|
Multiple Antennae |
Mx2 (for Signal Generators) |
MultHwMIMO_Mx2_2SG |
E4438C/N5182A |
|
2x2 MIMO Tx (for PXB) |
Source_N5106_HwSystem |
N5106A |