Installing the License in an M9383B VXG-m, M9384B VXG, and M9484C VXG Signal Generator

Before installing the license file, save a backup copy in a safe place.

Installing the License via a USB port

  1. Save the license file to the root directory of a USB storage device.

  2. Insert the storage device into a USB port of the PC or instrument matching the Host ID used in redemption.

  3. The license file should install automatically.

Installing the License via Keysight License Manager 5 (KLM5)

  1. On the PC or PC-based instrument matching the Host ID used in redemption, start the Keysight License Manager 5 (KLM5) software.

    You can download KLM5 at no charge from www.keysight.com/find/KLM5.

  2. From the KLM5 software, click the "Tools" icon > Install License File. Navigate to the license file and open it.

  3. The license file should install automatically.