Use this cell to enable or disable the fading channel for the 802.11n.
Use this cell to configure fading channel
parameters. When you click the
button in this cell, the Channel Configuration Dialog opens.
Choice: Constant | Frequency Dependent
Default: Constant
Select the IQ impairment mode. Each mode has a unique pair of impairment adjustments.
Constant -- IQ impairment is independent of frequency.
Frequency Dependent -- IQ impairment is a function of frequency with vector impairment adjustments applied to subcarriers.
This feature is only available for 802.11n with Option H and 802.11ac.
Use this cell to add quadrature skew impairment (-90 to + 90 degrees) to the generated waveform for the specific signal generator. This affects the waveform data so it applies to both RF and baseband I/Q outputs.This parameter is only available when the IQ Impairment Mode is set to Constant.
The baseband Quadrature Angle (angle) and the baseband IQ Gain (gain) values are used to modify the output I and Q data according to the following equations:
Real (output) = Real (input) - Gs * Imag (input)
Imag (output) = Gc * Imag\ (input)
where:
Gs = Gain * sin (angle) and
Gc = Gain * cos (angle)
Use this cell to add quadrature gain impairment (-10 dB to 10 dB) to the generated waveform for the specific signal generator. This affects the waveform data so it applies to both the RF and baseband I/Q outputs. This parameter is only available when the IQ Impairment Mode is set to Constant.
Default: all zeros
This is a vector with a maximum length of 512. Click
in the parameter field to open a
window where you can specify the quadrature angle for every subcarrier in the OFDM signal. ānā specifies the index of the antenna. When you click on the button at the rightmost side of the field, a window appears, allowing you enter a phase error for each subcarrier. This parameter is only available when the IQ Impairment Mode is set to Frequency Dependent.
Default: all zeros
This is a vector with a maximum length of 512. Click
in the parameter field to open a
window where you can specify the in-phase gain for every subcarrier in the OFDM signal. ānā specifies the index of the antenna. When you click on the button at the rightmost side of the field, a window appears, allowing you enter a phase error for each subcarrier. This parameter is only available when the IQ Impairment Mode is set to Frequency Dependent.