Double-click or use the drop-down menu to set the operating state of the selected feature.
On – enables the feature. If the state is on, but the connected instrument does not have the required license, the cell turns orange.
Off – disables the feature.
Displays the model number of the licensed feature.
The minor enhancement updates (MEU) option allows you to obtain the latest capabilities of the software. It is purchased as N7617B-MEU. However, each enhancement update is licensed as N7617B-Uxx, as shown in the image above. As more enhancements become available, the option suffix increments: U01, U02, U03 and so on. Purchasing MEU includes all the capabilities from previous MEU licenses. For example, purchasing the license for U03 includes everything that was in U01 and U02. If you had purchased an earlier MEU license, such as U01, and want the most recent MEU capabilities available in U03, purchasing another MEU license upgrades your software to the most current state.
| Release Date | Software Version | MEU License |
Minor Enhancements |
|---|---|---|---|
| Sep 2016 | 3.0 | U03 |
|
| Sep 2015 | 2.2 | U02 |
|
| Jan 2015 | 2.0 | U01 |
|
Displays a description of the licensed feature.
Displays the status of the selected feature on the connected instrument.
Valid – the license is installed and active.
Invalid – the license is expired.
N/A – the license is not applicable.
Info Not Available – the Signal Studio software does not provide license information for some products.
When a new instrument connection is established or the hardware configuration is changed, the instrument licenses are automatically retrieved from the connected instrument. If the connected instrument does not have the correct licensing for the current waveform setup, initial settings are restored. You are prompted to save the setup parameters before continuing.