Go to topic Go to topic Go to topic Go to topic Go to topic

8. Real-time Noise Setup

Real-time Noise features require connection to a signal generator with option 403.

Real-time Noise

Choice: On | Off

Default: Off

This cell enables or disables adding real-time, non-repeating additive white Gaussian noise (AWGN) to the carrier being modulated by the waveform being played.

Carrier to Noise Ratio

Range: –100 dB to 100 dB

Default: 20 dB

This cell selects the noise power to be applied to a waveform. The carrier power is defined as the total modulated signal power before noise power is added. The noise power is the in-channel noise power. A positive value makes C larger than N.

Carrier Bandwidth

Range: 1 Hz to 80.0 MHz

Default: 16.25 MHz

Sets the carrier bandwidth. This should be the same as the bandwidth of the target carrier.

Noise Bandwidth Factor

Range: 1 to 2

Default: 1

This cell displays the noise bandwidth factor. (Read-only).

The Noise Bandwidth is calculated as following:

The noise bandwidth is at least 0.8 * [ARB Sample Clock] * [Noise Bandwidth Factor]

This parameter is not available with all instrument model numbers and may be grayed out.

Noise Bandwidth

Range: 1 Hz to 100 MHz

Default: 1.0 Hz

This cell displays the noise bandwidth.

This parameter is not available with all instrument model numbers and may be grayed out.