Installation Steps: 1 2 3 4 5 6 7 8 9
If you are not using the Pulse Building software with an external Arb (M8190A, N603xA, M933xA, or N824xA), skip to Step 7.
If you are using Pulse Building software with an M8190A arbitrary waveform generator be sure that the M8190A firmware version 2.3.1.0 or later is installed and functional on the AXIe embedded controller or on the PC that is physically connected to the M8190A hardware.
M8190A Arbitrary Waveform Generator Firmware (installed on controlling PC)
Firmware version 2.3.1.0 or later. Requires Keysight IO Libraries version 18.0 or later.
If you are using Pulse Building software with an N603xA/M933xA arbitrary waveform generator, install M9330A IVI driver version 2.01.0001 or later on the PC connected to the N603xA/M933xA hardware.
M933xA/N603xA Arbitrary Waveform Generator IVI Drivers
The M9330A IVI driver version 2.01.0001 is used for the N603xA family of arbitrary waveform generators.
If you are using Pulse Building software with an N824xA arbitrary waveform generator, install N8241A IVI driver version 1.31.3 or later on the PC running the Pulse Building software.
N824xA Arbitrary Waveform Generator Synthetic Instrument Module IVI Drivers and Control Utility