Quick Setups

Selecting Quick Setups in the Closedtree view displays the quick setup icons to help you begin signal configuration. The software comes with a single, pre-configured Internal Arb quick setup for use in offline mode as a simulated hardware setup.

Save As Quick Setup

Click this Closedbutton to save the current configuration as a custom quick setup. A Closedwindow appears, enabling you to enter a name for the quick setup. 

Open Quick Setup

Highlight a Closedquick setup name in the list, then click this Closedbutton to open that quick setup.

Delete Quick Setup

Highlight a Closedquick setup name in the list, then right click and select ClosedDelete to delete that quick setup. This menu item is not available (grayed-out) if a quick setup cannot be deleted.

Rename Quick Setup

Highlight a Closedquick setup name in the list, then right click and select ClosedRename to rename that quick setup. This menu item is not available (grayed-out) if a quick setup cannot be renamed.