Tek-Arb Floating Source File Type

AWG520 internal formats (*.wfm)

This waveform file contains waveform data in single precision floating-point numbers and marker data. Details...

Example waveform file that contains two-point data.

I Source File

Enter the path to the I Source File you want to import, or select the I Source File field, then use the Browse button to open a dialog window, then navigate to the desired file.

Q Source File

Enter the path to the Q Source File you want to import, or select the Q Source File field, then use the Browse button to open a dialog window, then navigate to the desired file.

Number of Markers

Displays the number of markers defined in the imported waveform file. (Read-only)

Number of Points

Displays the number of points defined by the data files in the selected waveform. (Read-only)