Choice: Normal | Short
Default: Normal
Double-click or use the drop-down menu to select whether to use normal LDPC block size or short LDPC block size in DVB-T2.
Choice: 1/2 | 3/5 | 2/3 | 3/4 |4/5 | 5/6
Default: 1/2
Double-click or use the drop-down menu to select the LDPC code rate of DVB-T2.
Range: different setting has different range, the minimum is 1.
Default: 2
FEC block number in a T2 frame.
Choice: QPSK | 16QAM | 64QAM | 256QAM
Default: QPSK
Double-click or use the drop-down menu to select the modulation type.
Choice: True | False
Default: False
Double-click or use the drop-down menu to select the whether constellation rotated.
Range: 0 to FEC Block Number
Default: 1
Set the number of time interleaving blocks per interleaving frame. The value “0” means no time interleaving is applied.
Default: TYPE 0
This version only supports the TYPE 0.
Range: different setting has different range
Default: 1
This version only supports one IF per T2 Frame.
Show the PLP Number in one frame.
Range: 0 to 255
Default: 0
Set the PLP ID of this PLP.
Range: 0 to 255
Default: 0
The supported file size for current settings.
Set the PLP Group ID of this PLP.
The supported file size for current settings.
The payload settings.
Choice:
Normal: Test Pattern | Demo File | TS File | TS File Wizard
When RS Encoder is off: Test Pattern | TS File
For DVB-H: Test Pattern | TS File
For one-seg ISDB-T: Test Pattern | TS File | TS File Wizard
Default: Test Pattern
Double-click or use the drop-down menu to select which type to be used as the data source.
If "TS File" is selected, "File Name" is required; If "TS File Wizard" is selected, "File Wizard" is available.
The data bits used as test pattern.
Click the right button to open "Data Pattern Selection" dialog and select test pattern to use.
Choice: True | False
Default: False
Double-click or use the drop-down menu to determine whether a SYNC byte (0x47) should be inserted into the test pattern.