Range: 0 to 19
Default: 0
Gets the grant index of DOCSIS 4.0 Upstream carrier
Gets or sets the data payload for current grant. Click the right button to open payload dialog.
There are two radio buttons at the top of this dialog.
Gets or sets the frame start index of current grant. This parameter determines the start position of the grant from the angle of time domain.
Gets or sets the minislot start index of current grant. This parameter determines the start position of the grant from the angle of frequency domain.
Gets the total number of minislots in current grant.