|
1. DVB-T |
2. DVB-H |
3. Payload |
|---|---|---|
|
|
||
|
|
||
|
|
||
|
|
||
|
|
||
|
4. MultiPath |
||
Choice: 2K | 4K | 8K
Default: 2K
Double-click or use the drop-down menu to select the mode.
[:SOURce]:RADio:DVBT[:BBG]:NFFT N2K|N4K|N8K
[:SOURce]:RADio:DVBT[:BBG]:NFFT?
Choice: 5MHz | 6MHz | 7MHz | 8MHz
Default: 8MHz
Couplings: Sample Rate on Real Time BBG node is affected by changes to this cell.
Double-click or use the drop-down menu to select the bandwidth.
[:SOURce]:RADio:DVBT[:BBG]:BANDwidth BW8|BW7|BW6|BW5
[:SOURce]:RADio:DVBT[:BBG]:BANDwidth?
Choice: QPSK | 16 QAM | 64QAM
Default: QPSK
Double-click or use the drop-down menu to select the modulation type.
[:SOURce]:RADio:DVBT[:BBG]:MODUlation QPSK|QAM16|QAM64
[:SOURce]:RADio:DVBT[:BBG]:MODUlation?
Choice: 1/4 | 1/8 | 1/16 | 1/32
Default: 1/4
Double-click or use the drop-down menu to select the guard interval.
[:SOURce]:RADio:DVBT[:BBG]DVBT:GINTerval [GI4]|GI8|GI16|GI32
[:SOURce]:RADio:DVBT[:BBG]DVBT:GINTerval?
Choice: On | Off
Default: On
Double-click or use the drop-down menu to control the cell ID state.
[:SOURce]:RADio:DVBT[:BBG]CENable ON|OFF|1|0
[:SOURce]:RADio:DVBT[:BBG]CENable?
Range: 0 to 65535
Default: 0
Couplings: Displayed only when Cell ID Enabled is set to On.
Set the cell ID.
[:SOURce]:RADio:DVBT[:BBG]:CID <val>
[:SOURce]:RADio:DVBT[:BBG]:CID?
Choice: 1/2 | 2/3 | 3/4 | 5/6 | 7/8
Default: 1/2
Double-click or use the drop-down menu to select the code rate of convolutional coder.
[:SOURce]:RADio:DVBT[:BBG]:CRATe [R1BY2]|R2BY3|R3BY4|R5BY6|R7BY8
[:SOURce]:RADio:DVBT[:BBG]:CRATe?
Choice: On | Off
Default: On
Double-click or use the drop-down menu to select whether the baseband filter is enabled.
[:SOURce]:RADio:DVBT[:BBG]:FILTer ON|OFF|1|0
[:SOURce]:RADio:DVBT[:BBG]:FILTer?
Choice: On | Off
Default: Off
Double-click or use the drop-down menu to select if this configuration is DVB-H.
If this value is On, DVB-H TS files are required for payload.
[:SOURce]:RADio:DVBT[:BBG]:DVBH ON|OFF|1|0
[:SOURce]:RADio:DVBT[:BBG]:DVBH?
Choice: Native Interleaver | In-depth Interleaver
Default: Native Interleaver
Double-click or use the drop-down menu to select the interleaver.
[:SOURce]:RADio:DVBT[:BBG]:ILEaver [NATive]|INDepth
[:SOURce]:RADio:DVBT[:BBG]:ILEaver?
Choice: On | Off
Default: Off
Couplings: Displayed only when DVB-H Enabled is set to On.
Double-click or use the drop-down menu to select whether the time slicing flag is set in TPS.
[:SOURce]:RADio:DVBT[:BBG]:TSLIcing ON|OFF|1|0
[:SOURce]:RADio:DVBT[:BBG]:TSLIcing?
Choice: On | Off
Default: Off
Couplings: Displayed only when DVB-H Enabled is set to On.
Double-click or use the drop-down menu to select whether the MPE-FEC flag is set in TPS.
[:SOURce]:RADio:DVBT[:BBG]:MPEFec ON|OFF|1|0
[:SOURce]:RADio:DVBT[:BBG]:MPEFec?
Choice: Demo File| TS File | NULL TS Packet | Pattern |PN9 | PN15 | PN23
Default:Demo File
Double-click or use the drop-down menu to select which type to use as the data source.
[:SOURce]:RADio:DVBT[:BBG]:PAYLoad:TYPE DEMOfile|FILE|NULL|PATtern|PN9|PN15|PN23
[:SOURce]:RADio:DVBT[:BBG]:PAYLoad:TYPE?
Choice: Local| Instrument
Default: Local
Couplings: Displayed only when the Data Source Type is TS File.
Double-click or use the drop-down menu to set the TS file location to local computer or instrument. As a best practice, save the TS file to the local computer and set File Location to Local.
Couplings: Displayed only when the Data Source Type is TS File.
Click on the right side of the cell to browse your computer and
select the TS file.
[:SOURce]:RADio:DVBT[:BBG]PAYLoad:FILE <"filename">
[:SOURce]:RADio:DVBT[:BBG]PAYLoad:FILE?
Choice: NULL Packet Header (0x471FFF10) | SYNC Byte(0x47) | None
Default: SYNC byte (0x47)
Couplings: Displayed only when the Data Source Type is Pattern, PN9, PN15 or PN23.
Double-click or use the drop-down menu to determine whether a SYNC byte (0x47) or a NULL packet header(0x471FFF10) should be inserted into the test pattern.
[:SOURce]:RADio:DVBT[:BBG]:PAYLoad:SYNC NULL|BYTE|NONE
[:SOURce]:RADio:DVBT[:BBG]:PAYLoad:SYNC?
Couplings: Displayed only when the Data Source Type is Pattern.
Enter the data bits to use in a test pattern.
[:SOURce]:RADio:DVBT[:BBG]:PAYLoad:PATTern <val>
[:SOURce]:RADio:DVBT[:BBG]:PAYLoad:PATTern?
Choice: On | Off
Default: On
Couplings: Displayed only when the Data Source Type is Demo File or TS File.
Double-click or use the drop-down menu to enable or disable packet stuffing.
[:SOURce]:RADio:DVBT[:BBG]PAYLoad:STUFfing ON|OFF|1|0
[:SOURce]:RADio:DVBT[:BBG]PAYLoad:STUFfing?
Choice: On | Off
Default: On
Couplings: Displayed only when the Data Source Type is Demo File or TS File.
Double-click or use the drop-down menu to enable or disable PCR Adjust.
[:SOURce]:RADio:DVBT[:BBG]PAYLoad:PCRAdjust ON|OFF|1|0
[:SOURce]:RADio:DVBT[:BBG]PAYLoad:PCRAdjust?
Range: 0 to 10 MHz
Default: 0.0
Set the frequency for the PCR offset (the offset is calculated by the sin function).
[:SOURce]:RADio:DVBT[:BBG]:PAYLoad:PCRFrequency <val>
[:SOURce]:RADio:DVBT[:BBG]:PAYLoad:PCRFrequency?
Range: 0 to 10 us
Default: 0
Set the amplitude for the PCR offset (the offset is calculated by the sin function).
[:SOURce]:RADio:DVBT[:BBG]:PAYLoad:PCRAMplitude <val>
[:SOURce]:RADio:DVBT[:BBG]:PAYLoad:PCRAMplitude?
Couplings: Displayed only when the Data Source Type is Demo File or TS File.
Displays the useful bit rate for current setting.
[:SOURce]:RADio:DVBT[:BBG]PAYLoad:UBITrate?
Couplings: Displayed only when the Data Source Type is Demo File or TS File.
Displays the stream bit rate for current TS file.
[:SOURce]:RADio:DVBT[:BBG]PAYLoad:SBITrate?
Choice: Off | 1 Path | 2 Path | 3 Path | 4 Path
Default: Off
Click on the right side of the cell to open the Multi-path Channel dialog box. Use the dialog box to configure up to 4 static paths. For each path, you can set amplitude attenuation (r), time delay (t [ms]), phase offset (q [rad]), and frequency offset (w [kHz]).