|
1. DVB-C |
2. Payload |
3. MultiPath |
|---|---|---|
| Multi-path Channel | ||
|
|
||
|
|
||
|
|
||
| PCR Offset Frequency | ||
| PCR Offset Amplitude | ||
|
|
||
|
|
Choice: Root Nyquist | Nyquist
Default: Root Nyquist
Double-click or use the drop-down menu to select the filter type.
[:SOURce]:RADio:DVBC[:BBG]:FILTer RNYQ|NYQ
[:SOURce]:RADio:DVBC[:BBG]:FILTer?
Range: 0 to 1
Default: 0.15
Set the roll-off factor for DVB-C.
[:SOURce]:RADio:DVBC[:BBG]:ALPHa <val>
[:SOURce]:RADio:DVBC[:BBG]:ALPHa?
Choice: 16QAM |32QAM |64QAM |128QAM |256QAM
Default: 16QAM
Double-click or use the drop-down menu to select the modulation type.
[:SOURce]:RADio:DVBC[:BBG]:MODUlation QAM16|QAM32|QAM64|QAM128|QAM256
[:SOURce]:RADio:DVBC[:BBG]:MODUlation?
Range: 100 KSymbols/s to 10 MSymbols/s
Default: 6.900000 MSymbols/s
Set the symbol rate for DVB-C.
[:SOURce]:RADio:DVBC[:BBG]:SYMRate <val>
[:SOURce]:RADio:DVBC[:BBG]:SYMRate?
Choice: Demo File| TS File | NULL TS Packet | Pattern |PN9 | PN15 | PN23
Default:Demo File
Double-click or use the drop-down menu to select which type to use as the data source.
[:SOURce]:RADio:DVBC[:BBG]:PAYLoad:TYPE DEMOfile|FILE|NULL|PATtern|PN9|PN15|PN23
[:SOURce]:RADio:DVBC[:BBG]:PAYLoad:TYPE?
Choice: Local| Instrument
Default: Local
Couplings: Displayed only when the Data Source Type is TS File.
Double-click or use the drop-down menu to set the TS file location to local computer or instrument. As a best practice, save the TS file to the local computer and set File Location to Local.
Couplings: Displayed only when the Data Source Type is TS File.
Click on the right side of the cell to browse your computer and
select the TS file.
[:SOURce]:RADio:DVBC[:BBG]:PAYLoad:FILE "<file path/file name>"
[:SOURce]:RADio:DVBC[:BBG]:PAYLoad:FILE?
Choice: NULL Packet Header (0x471FFF10) | SYNC Byte(0x47) | None
Default: SYNC byte (0x47)
Couplings: Displayed only when the Data Source Type is Pattern, PN9, PN15 or PN23.
Double-click or use the drop-down menu to determine whether a SYNC byte (0x47) or a NULL packet header(0x471FFF10) should be inserted into the test pattern.
[:SOURce]:RADio:DVBC[:BBG]:PAYLoad:SYNC NULL|BYTE|NONE
[:SOURce]:RADio:DVBC[:BBG]:PAYLoad:SYNC?
Couplings: Displayed only when the Data Source Type is Pattern.
Enter the data bits to use in a test pattern.
[:SOURce]:RADio:DVBC[:BBG]:PAYLoad:PATTern <val>
[:SOURce]:RADio:DVBC[:BBG]:PAYLoad:PATTern?
Choice: On | Off
Default: On
Couplings: Displayed only when the Data Source Type is Demo File or TS File.
Double-click or use the drop-down menu to enable or disable packet stuffing.
[:SOURce]:RADio:DVBC[:BBG]:PAYLoad:STUFfing 0|1|ON|OFF
[:SOURce]:RADio:DVBC[:BBG]:PAYLoad:STUFfing?
Choice: On | Off
Default: On
Couplings: Displayed only when the Data Source Type is Demo File or TS File.
Double-click or use the drop-down menu to enable or disable PCR Adjust.
[:SOURce]:RADio:DVBC[:BBG]:PAYLoad:PCRAdjust 0|1|ON|OFF
[:SOURce]:RADio:DVBC[:BBG]:PAYLoad:PCRAdjust?
Range: 0 to 10 MHz
Default: 0.0
Set the frequency for the PCR offset (the offset is calculated using the sin function).
[:SOURce]:RADio:DVBC[:BBG]:PAYLoad:PCRFrequency <val>
[:SOURce]:RADio:DVBC[:BBG]:PAYLoad:PCRFrequency?
Range: 0 to 10 us
Default: 0
Set the amplitude for the PCR offset (the offset is calculated using the sin function).
[:SOURce]:RADio:DVBC[:BBG]:PAYLoad:PCRAMplitude <val>
[:SOURce]:RADio:DVBC[:BBG]:PAYLoad:PCRAMplitude?
Couplings: Displayed only when the Data Source Type is Demo File or TS File.
Displays the useful bit rate for the current setting.
[:SOURce]:RADio:DVBC[:BBG]:PAYLoad:UBITrate?
Couplings: Displayed only when the Data Source Type is Demo File or TS File.
Displays the stream bit rate for the current TS file.
[:SOURce]:RADio:DVBC[:BBG]:PAYLoad:SBITrate?
Choice: Off | 1 Path | 2 Path | 3 Path | 4 Path
Default: Off
Click on the right side of the cell to open the Multi-path Channel dialog box. Use the dialog box to configure up to 4 static paths. For each path, you can set amplitude attenuation (r), time delay (t [ms]), phase offset (q [rad]), and frequency offset (w [kHz]).