Click Licenses node in the
tree view
to display the window shown below.
Displays the licensed feature's index number.
Displays the license option name for the feature or the capability options available in the software. All capability and connectivity options are locked to the target instrument. Feature capability is either Basic or Advanced. Feature connectivity is specific to the type of signal generator. The option number identifies the type of license, whether perpetual or time-based, fixed or transportable, and so on.
The minor enhancement updates (MEU) option allows you to obtain the latest capabilities of the software. It is purchased as N7623B-MEU. However, each enhancement update is licensed as N7623B-Uxx, as shown in the image above. As more enhancements become available, the option suffix increments: U01, U02, U03 and so on. Purchasing MEU includes all the capabilities from previous MEU licenses. For example, purchasing the license for U03 includes everything that was in U01 and U02. If you had purchased an earlier MEU license, such as U01, and want the most recent MEU capabilities available in U03, purchasing another MEU license upgrades your software to the most current state.
| Release Date | Software Version | MEU License |
Minor Enhancements |
|---|---|---|---|
| Aug 2013 | 6.2 | U01 |
|
Double-click or use the drop-down menu to set the operating state of the selected feature.
On – enables the feature.
Off – disables the feature.
The State cell color changes to red if a feature is set to On and there is not a valid license available, or the license is expired.
Displays the descriptive information of the licensed feature.
Displays the status of the selected license on the connected instrument.
– the license is installed and active.
– the license is expired or not installed.
– the license is not applicable.
When a new instrument connection is established or the hardware configuration is changed, the instrument licenses are automatically retrieved from the connected instrument. If the connected instrument does not have the correct licensing for the current waveform setup, initial settings are restored. You are prompted to save the setup parameters before continuing.
Displays the name of the carrier associated with the selected feature.
Displays the status of the carrier.
– the carrier is available for use.
– the carrier is not available or the license is not active.
Displays the name of the feature required for the selected instrument.