Real Time

Printing Popup Topics

The Popup Text Prints Over Existing Topic

When you click the print icon while a popup is active, the printer prints the popup text over the existing topic text. The popup text has to be printed separately from the topic text. This procedure demonstrates how to print the popup text separately.

  1. Activate the popup.

  2. Move the cursor over the popup text.

  3. Right-click.

    If the popup closes, reopen it and make sure that the cursor is over the popup when you right-click.

  4. From the menu that appears, choose Print.