Viewing Parameter Descriptions
Resizing Window Panes and Cell Columns
Collapsing and Expanding Tables
Check
in the upper right corner of a parameter configuration window
to display the
cell description window,
and then click a parameter cell to display a brief description. The initial
state is unchecked.
The software interface uses cells (similar to a spread sheet) for configuring various parameters. Some cells have discrete settings; others are arbitrary. For example, RF Output uses discrete settings. You must select from either On or Off.
, on the other hand, uses arbitrary settings. You can enter any value within the designed range.
, double click either the cell with the name of the parameter, or the setting. This highlights the current setting. Enter the new value. You do not need to type "MHz"; the letter "m" is sufficient. The same is true for GHz and kHz. Without "k", "m" or "g", the default frequency is 100.000 000 kHz.
The left pane of the main window is called the
tree view.
It is useful for navigating between the quick setups, hardware
configuration and signal generator settings, and the Waveform
Setup. The right pane of the main window is called the
Parameter view.
This area enables you to select the project parameters and signal generator
settings for displaying the waveform. Selecting an item in the tree view
enables the related elements in the parameter view.
You can resize window panes and cell columns for
better viewing. As you move the mouse pointer over a border, it changes
form, indicating that the border can be moved
horizontally
or
vertically.
Hold down the left mouse button and drag the border to its new position.
To create more viewing space in a window pane, you can collapse selection
tables you are not using. Click the minus box next
to the title of the table and the table collapses. Click the plus
box and it expands
again.