DVB-S

1. DVB-S

2. Payload

3. MultiPath

Filter Type

Data Source Type

Multi-path Channel

Roll-off Factor

File Location

 

Symbol Rate

File Name

 

Code Rate

Sync Insert

 

 

Pattern Bits

 

 

Packet Stuffing

 

 

PCR Adjust

 
  PCR Offset Frequency  
  PCR Offset Amplitude  

 

Useful Bit Rate

 

 

Stream Bit Rate

 

1. DVB-S

Filter Type

Choice: Nyquist |Root Nyquist

Default: Root Nyquist

Double-click or use the drop-down menu to select the filter type for DVB-S.

Roll-off Factor

Range: 0 to 1

Default: 0.35

Set the roll-off factor for DVB-S.

Symbol Rate

Range: 100kSymbols/s to 50MSymbols/s

Default: 25.000000 MSymbols/s

Set the symbol rate for DVB-S.

Code Rate

Choice: 1/2 | 2/3 | 3/4 | 5/6 | 7/8

Default: 1/2

Double-click or use the drop-down menu to select the code rate for DVB-S.

2. Payload

Data Source Type

Choice: Demo File| TS File | NULL TS Packet | Pattern |PN9 | PN15 | PN23

Default:Demo File

Double-click or use the drop-down menu to select which type to use as the data source.

File Location

Choice: Local| Instrument

Default: Local

Couplings: Displayed only when the Data Source Type is TS File.

Use "Local" as the File Location and note that "Instrument" is not supported in PXB.

File Name

Couplings: Displayed only when the Data Source Type is TS File.

Click on the right side of the cell to browse your computer and select the TS file.

Sync Insert

Choice: NULL Packet Header (0x471FFF10) | SYNC Byte(0x47) | None

Default: SYNC byte (0x47)

Couplings: Displayed only when the Data Source Type is Pattern, PN9, PN15, or PN23.

Double-click or use the drop-down menu to determine whether a SYNC byte (0x47) or a NULL packet header(0x471FFF10) should be inserted into the test pattern.

Pattern Bits

Couplings: Displayed only when the Data Source Type is Pattern.

Enter the data bits to use in a test pattern.

Packet Stuffing

Choice: On | Off

Default: On

Couplings: Displayed only when the Data Source Type is Demo File or TS File.

Double-click or use the drop-down menu to enable or disable packet stuffing.

PCR Adjust

Choice: On | Off

Default: On

Couplings: Displayed only when the Data Source Type is Demo File or TS File.

Double-click or use the drop-down menu to enable or disable PCR Adjust.

PCR Offset Frequency

Range: 0 to 10 MHz

Default: 0.0

Set the frequency for the PCR offset (the offset is calculated by the sin function).

PCR Offset Amplitude

Range: 0 to 10 us

Default: 0

Set the amplitude for the PCR offset (the offset is calculated by the sin function).

Useful Bit Rate

Couplings: Displayed only when the Data Source Type is Demo File or TS File.

Displays the useful bit rate for the current setting.

Stream Bit Rate

Couplings: Displayed only when the Data Source Type is Demo File or TS File.

Displays the stream bit rate for the current TS file.

3. MultiPath

Multi-path Channel

Choice: Off | 1 Path | 2 Path | 3 Path | 4 Path

Default: Off

Click on the right side of the cell to open the Multi-path Channel dialog box. Use the dialog box to configure up to 4 static paths. For each path, you can set amplitude attenuation (r), time delay (t [ms]), phase offset (q [rad]), and frequency offset (w [kHz]).