To generate signals using the N7624C Signal Studio Pro for LTE/LTE-Advanced FDD 2027 software, you must have a properly configured PC and a properly configured instrument, as described in the following table.
|
Instruments |
Requirements |
|---|---|
|
N5186A MXG vector signal generator |
Firmware:
|
|
N5172B EXG X-Series RF vector signal generator |
Firmware:
Required options:
Recommended options:
|
|
N5182B MXG X-Series RF vector signal generator |
Firmware:
Required options:
Recommended options:
|
|
N5166B CXG RF vector signal generator |
Firmware:
|
|
N5182A MXG vector signal generator NOTE: This instrument model is valid only when Playback License Mode is set to PC License. |
Firmware:
Required options:
Recommended options:
|
|
E4438C ESG vector signal generator NOTE: This instrument model is valid only when Playback License Mode is set to PC License. |
Firmware:
Required options:
Recommended options:
|
|
E8267D PSG vector signal generator |
Firmware:
Required options:
Use power search with ALC turned off to get accurate power. |
|
M9381A PXIe vector signal generator (single-channel configurations) |
Driver:
Recommended options:
Additional options to consider:
Limitations: The M9381A VSG has a limitation related to the Power Search and DC Cal functions, creating a time-synchronization loss. That is, the signal timing changes after a Power Search or DC Cal. When ALC is set to Off, Signal Studio automatically runs Power Search, which affects the user's trigger signal for starting waveform playback. Even though the timing alignment of the trigger signal and waveform are properly set, the Power Search function disrupts this synchronization. In these cases, use the following workarounds:
For DC Cal, run it before you download and play the waveform. Do not run DC Cal while the signal is playing, which disrupts the synchronization. |
|
M9381A PXIe vector signal generator (multichannel synchronization) |
Driver:
Required options:
Required for 8-channel configurations:
Recommended options:
Limitations: The M9381A VSG has a limitation related to the Power Search and DC Cal functions, creating a time-synchronization loss. That is, the signal timing changes after a Power Search or DC Cal. When ALC is set to Off, Signal Studio automatically runs Power Search, which affects the user's trigger signal for starting waveform playback. Even though the timing alignment of the trigger signal and waveform are properly set, the Power Search function disrupts this synchronization. In these cases, use the following workarounds:
For DC Cal, run it before you download and play the waveform. Do not run DC Cal while the signal is playing, which disrupts the synchronization. |
|
M9383B VXG-m microwave signal generator |
Firmware:
Recommended options:
|
|
M9384B VXG microwave signal generator |
Firmware:
Recommended options:
|
|
M9484C VXG signal generator |
Firmware:
|
|
M8190A arbitrary waveform generator |
Firmware:
Required options:
Recommended options:
|
|
E6640A EXM wireless test set |
Software:
Recommended options:
Additional options to consider:
|
|
M9420A VXT PXIe vector transceiver |
Software:
Recommended options:
Additional options to consider:
|
|
M9421A VXT PXIe vector transceiver |
Software:
Recommended options:
Additional options to consider:
|
|
Solution |
Instruments |
Requirements |
|---|---|---|
|
Solution without Baseband Timing Alignment and RF Phase Coherence (Two signal generators driven from 10 MHz reference and the same trigger) |
Two N5172B EXGs Two E4438C ESGs |
N5172B EXG, N5182B MXG, and E4438C ESG: Same requirements as single antenna (see table above) |
|
Solution with Baseband Timing Alignment, but without RF Phase Coherence (Two signal generators with baseband generator clock coherence, but without RF common LO) |
Two N5172B EXGs Two N5182B MXGs -or-
|
N5172B EXG, N5182B MXG, and N5182A MXG: Same requirements as single antenna (see table above)
E4438C ESG: Same requirements as single antenna (see table above), plus E4438C-HEC (provides external baseband generator clock input, which requires 200 - 400 MHz clock input signal) |
|
One external ARB clock |
Working with E4438C ESG: N5181A with Option 501 (MXG analog signal generator, 250 KHz to 1 GHz) |
|
|
Solution with Baseband Timing Alignment and RF Phase Coherence (Two signal generators with RF common LO and baseband generator clock coherence) |
Two N5172B EXGs -or- Two E4438C ESGs |
N5172B EXG, N5182B MXG, and N5182A MXG: Same requirements as single antenna (see table above), plus N5182A-012 (LO IN/OUT for phase coherency)
E4438C ESG: Same requirements as single antenna (see table above), plus E4438C-HEC (provides external baseband generator clock input, which requires 200-400 MHz clock input signal) E4438C-HCC (provides 250 MHz to 4 GHz IN & OUT on the rear panel of the E4438C) E4438C-HBC (provides 4 GHz to 6 GHz IN & OUT on the rear panel of the E4438C, requires E4438C-HCC and E4438C-506, I-bar OUT and Q-bar OUT connectors will be removed from the rear panel) |
|
Lock box plus external ARB clock or amplifier distribution |
Working with E4438C ESG: Z5623A-K10 (4-channel distribution amplifier, 250 MHz to 6 GHz) plus an N5181A with Option 501 (MXG analog signal generator, 250 kHz to 1 GHz) |
|
Solution |
Instruments |
Requirements |
|---|---|---|
|
All Real-Time MIMO Configurations |
Multiple N5172B EXGs |
Firmware: Version B.01.51 or later Required options: N5172B-660 (upgrade baseband generator with real-time capability |
To use the MSR feature you must have a properly configured instrument and software capabilities, as described in the table below. In addition, note the following:
MSR is a free upgrade to customers who have Basic capability (applies only to the N7624C and N7625C).
Waveforms created with the E4438C's embedded applications (Options 400, 401, and 402) are not compatible with the MSR feature.
|
Export/Import Software1 |
Instruments |
Hardware Requirements |
|---|---|---|
|
N7600C W-CDMA/HSPA+ N7601C cdma2000/1xEV-DO N7602C GSM/EDGE/Evo N7612C TD-SCDMA/HSDPA N7617C WLAN2 N7625C LTE/LTE-Advanced TDD3 N7626C V2X3 N7631C 5G NR |
N5182B MXG |
Best results require: N5182B-656 N5182B-023 N5182B-UNV MSR requires a minimum sample clock rate of 30.72 MHz. Refer to the N7624C technical overview for more information. |
|
N5172B EXG |
Best results require: N5172B-655 N5172B-022 N5172B-UNV MSR requires a minimum sample clock rate of 30.72 MHz. Refer to the N7624C technical overview for more information. |
|
|
N5182A MXG |
N5182A-652 or -654 N5182A-019 N5182A-UNV For firmware versions < C.01.60, N5182A-R2C, Internal Channel Correction, is required. N5182A-651 is not supported because MSR requires a minimum sample clock rate of 30.72 MHz. Refer to the N7624C technical overview for more information. |
|
|
E4438C ESG |
E4438C-503, -504, or -506 E4438C-601 or -602 |
|
|
M8190A AWG |
Refer to the M8190A hardware requirements above. |
1. You must purchase a valid Signal Studio software license for each of the component waveforms you want to use with the MSR feature.
2. Supports high-resolution waveform export.
3. Supports high-resolution waveform import/export.
|
Waveform |
Bandwidth |
Number |
Physical Memory |
Additional HDD Space Required |
|---|---|---|---|---|
|
10 ms |
20 MHz |
25 |
1 GB |
0.1 GB |
|
100 ms |
20 MHz |
100 |
2 GB |
4 GB |
|
160 ms |
20 MHz |
100 |
7 GB |
5 GB |
200 GB HDD with 2 GB free disk space at runtime (5 GB or higher recommended)
1024 x 768 screen resolution (1280 x 1024 recommended)
If you use a high-resolution display, the GUI's font size may appear too small to read. To resolve this, lower your PC's display resolution, but make sure the display scaling remains set at 100 percent, otherwise portions of the GUI will become truncated and hidden from view.
Windows 10 (64 bit):
1 GHz or faster
8 GB of memory minimum
1.5 GB hard disk space (includes 1 GB for Microsoft .NET Framework and 65 MB for the Keysight IO Libraries)
Microsoft Internet Explorer 11.0 or later
128 MB graphics memory with DirectX 9 graphics support (recommended)
Microsoft .NET Framework 4.6 or later
Keysight IO Libraries, version 18.0 or later
Keysight License Manager 5 (4. Downloading and Installing Keysight License Manager 5)
Keysight License Service (included with installer)
Keysight Host Processor Platform (included with installer)
Installed GPIB IO interface card, LAN interface card, or USB/GPIB interface connector
Keysight VISA
Microsoft Windows Installer version 2.0 or later