API commands for controlling the N7624C Signal Studio graphical user interface are documented in the N7624C Documented Class Library (N7624api.chm). This help file is located in the following directory:
C:\Program Files\Keysight\Signal Studio Pro\LTE-LTE-Advanced FDD 2020.0320
Many of the links in the API help require the Microsoft Visual Studio .NET integrated development environment (IDE). Without the IDE, these links appear broken. Download the IDE to repair the links.
The software installation includes Sample API Programs. You can use these samples as a starting point to develop your own API programs.
This software recognizes only US style numeric format, for example, floating point is "."
You must set the API locale to "en-US" using the following commands prior to starting the user main routine:
Thread.CurrentThread.CurrentCulture = new CultureInfo("en-US"); // Sets the culture to English (US)
Thread.CurrentThread.CurrentUICulture = new CultureInfo("en-US"); // Sets the UI culture to English (US)
You can see these culture setting commands in Main .cs, located in the ...\Samples\SimpleControl folder (See Sample API Programs).
The .NET Framework 4.x allows you to load pure managed assemblies built in any version of the .NET Framework. However, for some Signal Studio applications, API usage involves assemblies that are not pure .NET CLR. In these cases, you must configure your program (e.g. User_App.exe) to load .NET mixed-mode assemblies using the following steps:
Open a text editor.
Copy the following text into the text editor:
<?xml version="1.0" encoding="utf-8"?>
<configuration>
<startup useLegacyV2RuntimeActivationPolicy="true">
<supportedRuntime version="v4.0" />
</startup>
</configuration>
Save this new configuration file in the same directory as User_App.exe. Name the file User_App.exe.config.
Re-launch User_App.exe.
If you are using a recent version of Visual Studio, such as VS 2015, the default .NET version will be later than .NET 3.5, which is required for using the Signal Studio API. In this case, if you change the project settings of the Visual Studio program to .NET 3.5, you will not benefit from the latest .NET features. Therefore, it is better to create a .config file in your VS project, enabling you to benefit from the latest .NET features. To do this, follow the exact same steps described in Loading .NET Mixed-Mode Assemblies above.
The Microsoft.NET home page.
Developing Microsoft.NET Skills.
"Migrating Native Code to the .NET CLR," by Don Box.
Troelsen, Andrew. C# and the .NET Platform. New York: Apress, 2001.